Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Siemens launches world’s first 1200 kV SF6 Circuit Breaker

India’s growing economy needs an efficient power transmission system to meet the increasing demand for reliable and affordable power. With the 1200 kV system, India will leapfrog into a new transmission age that will contribute to the nation’s economic growth, with an objective to bring electricity across the nation. 
As an innovation-led technology leader, Siemens has opened up a new dimension in the high-voltage power transmission technology with the introduction of 1200 kV SF6 Circuit Breaker. Spanning over long distances and with a transmission capacity of 8000 megawatts (MW), the new 1200 kV system will have low transmission losses. 
The power transmission capacity of the 1200 kV line will be more than double as compared to the 800 kV line. This technology will make it possible to evacuate large amount of electric power from distant generating stations to load centers by interconnecting regional grids. The new 1200 kV system will need less than half the space used by the existing 800 kV system with fewer numbers of lines for transmitting the same power, thus reducing the land footprint and overall environmental impact. 
Siemens technology is creating new benchmarks in enabling efficient transmission of electricity. 
The 1200 kV Circuit Breaker was handed over to Shri. R. N. Nayak Chairman & MD, Power Grid Corporation of India Limited at Siemens manufacturing facility at Aurangabad. 
Dr. Armin Bruck, Managing Director, Siemens Ltd., said while dedicating the 1200 kV SF6 Circuit Breaker to the nation, “Siemens has always been known for pioneering innovation and technological leadership. The launch of the 1200 kV SF6 Circuit Breaker is a significant milestone in this journey. Contributing towards sustainable development of the nation’s economy by enhancing efficiency of the power sector is at the top of our agenda.”  
Mr. A. K. Dixit, CEO Energy Sector, Siemens Ltd., said, “With this technological advancement, power transmission over long distances will be more efficient while increasing the transmission capacity. Once installed, the 1200kV system will spare more land for alternative use.”

For this press release

 

Contact

Dr. Armin Bruck, Managing Director

Siemens Ltd.

130, Pandurang Budhkar Marg, 
Worli, Mumbai - 400 018. 
India

Tel. : (022) 3967 7000

Fax : (022) 3967 7500

Mr. Viswakumar Menon

Corporate Communication - Press Office

130, Pandurang Budhkar Marg,                                Worli, Mumbai - 400 018. 
India

Tel. : (022) 3967 7537 / 3967 7026

Fax : (022) 3967 7174