[{"name":"Home","site_name":"Press | Company | Siemens","description":"","url_str":"\/in\/","level":0,"image":"","base_root":"https:\/\/press.siemens.com","base_nid":"221","base_nodepath":"\/node\/221","base_path":"\/in\/","base_secure_url":"https:\/\/press.siemens.com\/in","children":null}]
It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and
usability.
For the best experience we suggest that you download the newest version of a supported browser:
Siemens Limited wins Rs. 271-crore order from Rashtriya Ispat Nigam Ltd.
Contract for complete renewal of blast furnace No. 2. Volume and production capacity will be increased significantly.
Contract for complete renewal of blast furnace No. 2. Volume and production capacity will be increased significantly.
A consortium comprising Siemens AG and Siemens Ltd. has received an order from the state-owned Rashtriya Ispat Nigam Ltd. (RINL) to thoroughly modernize blast furnace No. 2 at Visakhapatnam Steel Plant (Vizag Steel). The share of the order value for Siemens Limited is Rs. 271 crores.
Modernization will boost the furnace's inner volume from 3,200 to 3,820 cubic meters and production increase from 1.7 million tons per annum (MTPA) to 2.5 million tons per annum.
Visakhapatnam Steel Plant, which was founded in 1990 on the coast of the Indian federal state of Andhra Pradesh, is an integrated steelworks with an annual capacity of around 6.3 million tonnes of crude iron. Modernization of the blast furnaces is part of an expansion project which is intended to boost annual pig iron production to 7.3 million tonnes. Vizag Steel currently operates three blast furnaces: two with an interior volume of 3,200 cubic meters and one with interior volume of 3800-cubic meter. Blast furnace No. 2, which was constructed in 1992, has a nominal annual capacity of 1.7 million tonnes of crude iron.