Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Siemens and Sumitomo Electric win order for HVDC link

A consortium of Siemens and Sumitomo Electric Industries Ltd. has been awarded an order f rom Power Grid Corporation of India, the central transmission utility of India, to supply a high-voltage direct current (HVDC) transmission system. The total size of the order won by the consortium is US $520 million, of which the share of Siemens Limited is approximately Rs 1,682 crore.
"The grid-augmentation project will go a long way in delivering reliable, uninterrupted power to the state of Kerala. This project further demonstrates Siemens’ commitment to partner with the Government of India in its vision of delivering 24/7 power for all. The availability of reliable power transmission is key for India’s sustainable progress. Most of the critical equipment for the project is being sourced from factories in India, renewing our commitment towards Make in India," said Sunil Mathur, Managing Director and Chief Executive Officer, Siemens Limited.
The about 200-kilometer-long HVDC connection will be India’s first direct current link using voltagesourced converter (VSC) technology. VSC is the latest innovation in HVDC technology offering a very stable and highly-flexible reactive power control independent of active power control and additional features to support the AC systems like blackstart capability. Furthermore, this solution is ideal to be combined with XLPE cable technology.​
Siemens will be supplying two converter stations with two parallel converters, each rated 1000 Megawatts (MW), using its VSC HVDC technology while Sumitomo Electric will be responsible for XLPE HVDC cables in the DC circuit. The grid connection is scheduled to go into operation in the first half of 2020.

The Pugalur-Thrissur ±320 kilovolt (kV) HVDC system will connect Pugalur in the southern state of Tamil Nadu to Thrissur in Kerala State in South-West India. The Thrissur converter station will be connected via underground XLPE HVDC cable to a transition station also being built by Siemens. Sumitomo Electric's DC-XLPE cable has unique characteristics among industries to maximize utilization of HVDC system, enabling normal operation temperature at 90 degree and polarity reversal operation, which is suitable for future hybrid system with bulk power overhead line. Sumitomo Electric will supply 128km XLPE HVDC cables comprising four cables for a route of 32km. From the converter station at Pugalur, power will be transmitted via an overhead line to the transition station. The Siemens scope of supply for the turnkey project encompasses design, engineering, supply, installation as well as commissioning and major equipment supplies of the complete HVDC stations, including converter valves, transformers, cooling systems and control and protection technology. 

For this press release

 

Contact

Bijesh Kamath

Siemens Ltd., Media Relations

phone: +91 22 3967 7537, 3967 7000