Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release12 March 2019Siemens AGAthens
Siemens to show comprehensive portfolio for smart buildings
Building Technologies will present at ISH a variety of new cloud offerings, ranging
from cloud connectivity solutions to cloud operations. Any building site or device can
now be connected to the cloud easily and securely through the new Connect X300
gateway. This enables service companies, real estate managers, installers and
solution providers to benefit from digitalization and modernize their business
processes. Building Operator, the new cloud application, allows any of the
connected sites or devices to be monitored and controlled remotely.
Building Operator, as well as established cloud solutions such as Synco IC and
Climatix IC, are now powered by MindSphere. As a result, existing customers can
benefit from innovations on the MindSphere platform as well.
Building Technologies will also exhibit a new version of its Desigo CC integrated
building management platform which offers extended functionality. Highlights of
Desigo CC V4 include connectivity enhancements supporting data transmission with
KNX and M-Bus protocols for seamless integration, and the Flex Client, a new and
easier-to-use remote operation client option based on HTML5 technology.
Additionally, Building Technologies will demonstrate Desigo CC’s new extended
power management functionalities for better power quality and demand optimization.
Desigo CC Compact, which was launched in the fall of 2018, will make its trade fair
debut. The compact version of Desigo CC includes all essential features in one
software package and was specially developed to meet the functional requirements
of small and mid-size buildings. It makes it possible to operate different building
systems on one intuitive user interface, enhances transparency and increases the
productivity of building operations. Utilizing the modular Desigo CC platform, Desigo
CC Compact is adaptable and can be expanded as needed.
Complementing its portfolio of intelligent devices, Building Technologies will display
the new Intelligent Valve range. These self-optimizing, dynamic valves with cloud
connection for heating groups and air handling units optimize operation and
increase energy efficiency. The devices control the flow rate, measure temperature
and output, and adjust the valve settings to the heat exchanger. The Intelligent
Valves can be configured in the cloud and then put into operation quickly and
reliably through an app and Wi-Fi. The devices can be mounted flexibly and aligned
to the space available. The flow sensor, valve and controller box can be mounted
separately. The ability to load additional functions from the cloud at any time
ensures that the Intelligent Valve is always up to date.
Actuating DXR, a recent addition to the successful Desigo Room Automation
portfolio, combines a room controller with a damper actuator for variable air volume
(VAV) and fan-powered box applications in a single, compact unit. Consolidating the
two products into one appliance reduces the installation time and cost because no cabling is required between the controller and damper actuator, and only one device
needs to be mounted.
A dedicated engineering corner will show a set of products, applications and tools
for efficient engineering, commissioning, reporting and maintenance of Building
Technologies’ products and solutions. ABT Site is the engineering tool used for
building automation systems from Siemens, while ABT Go is available as a mobile
application for additional on-site efficiency.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Elisavet-Vasiliki Sachinidou
Siemens S.A.
Agisilaou 6-8
Marousi Athens
Marousi Athens
210 68.64.267