Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release19 May 2020Νυρεμβέργη
New 80 GHz compact radar transmitters for hassle-free level measurement
Siemens presents Sitrans LR100 series 80 GHz radar transmitters, compact instruments with a narrow beam for flexible installations in existing vessel openings—or even non-intrusively through plastic vessels. The transmitters’ 80GHz high frequency delivers robust, reliable measurements even in challenging environments such as those with vapors, condensation, turbulence, or solids. The custom microchip technology delivers fast response and extremely high sensitivity to detect even the weakest of signals.
The series consists of three products: Sitrans LR100 for basic measurement to 8 meter, Sitrans LR110 with communication and hazardous approvals options and range to 15 meter, Sitrans LR120 with communication, longest range to 30 meter and optional submergence shield for flooding protection. 2-wire loop powered with HART or optional Modbus RTU connectivity consumes very low energy and the fast start up is ideal for CSO (combined sewer overflow) applications.
The transmitters’ dependable readings reduce workers' exposure to hazardous situations: no need to climb tanks, lean out over sumps, or crawl into confined spaces to maintain instruments. As well, zero-meter blanking distance allows measurement right up to the sensor, thereby avoiding costly overfilling. And two-millimeter accuracy enhances operational safety through precise measurement through the full range of the application.
All this robust performance is wrapped in an IP68 submersible housing constructed of corrosion resistant PVDF. Simple commissioning is achieved with the Bluetooth interface and the Sitrans mobile IQ App or the Sitrans RD150 remote display. In remote areas connected to the Sitrans RTU3030C remote terminal unit, critical data can be transmitted as well as remote servicing can be performed.
Integrating critical level readings or process control data into operations can unlock new opportunities to react to safety concerns, analyze processes and identify areas for improvement. Users can monitor level measurements or diagnostic and maintenance information from the comfort of the control room or connect to Siemens MindSphere, the cloud-based, open IoT operating system.
Follow us on Twitter
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 76,000 employees internationally.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of intelligent infrastructure for buildings and distributed energy systems, and automation and digitalization in the process and manufacturing industries. Through the separately managed companies Siemens Energy, the global energy business of Siemens, and Siemens Mobility, a leading supplier of smart mobility solutions for rail and road transport, Siemens is shaping the energy systems of today and tomorrow as well as the world market for passenger and freight services. Due to its majority stakes in the publicly listed companies Siemens Healthineers AG and Siemens Gamesa Renewable Energy (as part of Siemens Energy), Siemens is also a world-leading supplier of medical technology and digital healthcare services as well as environmentally friendly solutions for onshore and offshore wind power generation. In fiscal 2019, which ended on September 30, 2019, Siemens generated revenue of €86.8 billion and net income of €5.6 billion. At the end of September 2019, the company had around 385,000 employees worldwide. Further information is available on the Internet www.siemens.com
Contact
Elisavet-Vasiliki Sachinidou
Siemens SA
Agisilaoy St. 6-8
Marousi, Athens
Postal Code: 151 23
Greece
Marousi, Athens
Postal Code: 151 23
Greece
(+30) 210-6864267