Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release23 May 2022Siemens AGNuremberg
Flexible, fast, and sustainable with the comprehensive digital twin for intralogistics
At Logimat, Siemens will use a Dynamic Gapper application to demonstrate how a digital twin helps to meet new intralogistics demands. In this typical intralogistics application, two upstream conveyors bring parcels of different sizes and not uniformly seperated onto a common conveyor belt, where the parcels are then being placed and separated within the right defined distance between each other. The technology company shows both the real application and its simulation. The precise simulation takes place before the actual construction is started. This allows the application to be virtually optimized and validated, which reduces the development and engineering time for machine builders by up to 35 percent. Operators of logistics centers also benefit from the digital twin, because with its help commissioning times can also be reduced by up to 40 percent. The entire hardware as well as the control system with all functions including communication, safety and web server can be simulated as part of a virtual commissioning. In the meantime, the real application can be built and wired and is ready for the actual commissioning. This then mainly consists of loading the program into the CPU and transferring the parameters to the drives.
The real application can also be further optimized during operation. By connecting to a cloud or edge platform, valuable process data can be collected and analyzed during operation. This enables operators of intralogistics centers to respond quickly to changes such as increased delivery volumes and create sustainable, flexible and scalable processes.
Siemens supports machine builders and operators of logistics centers on the path to digital transformation. The Digital Enterprise Portfolio offers an integrated product portfolio of software-based systems and automation technologies at the center of which is the digital twin. By using the digital twin of material handling equipment, warehouse operations and performance, the entire value chain is simulated and validated and can thus be designed optimally and efficiently. This consistently increases the efficiency of machine and plant construction and operation, minimizes error rates and downtimes, and shortens development times. Through the seamless interaction of the real and digital worlds, the technology company helps to increase the productivity and flexibility of plants and thus sustainably reduce the costs and energy consumption of logistics centers.
Further information on Siemens at Logimat please see www.siemens.com/press/intralogistics and www.siemens.com/logimat
Follow us on Twitter
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 72,000 employees internationally.
Siemens AG (Berlin and Munich) is a technology company focused on industry, infrastructure, transport, and healthcare. From more resource-efficient factories, resilient supply chains, and smarter buildings and grids, to cleaner and more comfortable transportation as well as advanced healthcare, the company creates technology with purpose adding real value for customers. By combining the real and the digital worlds, Siemens empowers its customers to transform their industries and markets, helping them to transform the everyday for billions of people. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a globally leading medical technology provider shaping the future of healthcare. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the transmission and generation of electrical power. In fiscal 2021, which ended on September 30, 2021, the Siemens Group generated revenue of €62.3 billion and net income of €6.7 billion. As of September 30, 2021, the company had around 303,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Elisavet-Vasiliki Sachinidou
Siemens A.Ε.
6-8 Agisilaou Str.
151 23, Μaroussi
Greece
151 23, Μaroussi
Greece
(+30) 210-6864267