Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release02 March 2021Smart InfrastructureMunich
New Siemens actuator line for small valves operates as quiet, connected multitasker
Simplified installation, fast commissioning
As the cold season has arrived and people spend more time indoors, heating needs to be efficiently controlled. The updated SSA actuators are well-suited to meet this demand with ease of installation and operation. All new actuators are delivered pre-configured and are ready for immediate installation. The newly introduced IP54 protection rating enables all installation directions, including overhead installations, for greater versatility. The new LED status display on the SSA actuators ensures fast and error-free commissioning. It shows the position of the valve and different operating states, while helping users with various functions, such as self-calibration. The latter is particularly important in the event of power failure, where proper operation can be restored without technical support or manual intervention. This allows building occupants a comfortable stay without interruptions. In addition, self-calibration offers automatic stem end position recognition and ensures that the actuator always fits the valve correctly which leads to precise regulation and energy savings.
High-class features for more applications
With new functionalities such as feedback signal and the possibility of switching to manual mode, operation has never been easier, time saving and cost efficient for the user. Thanks to manual operation or override, testing of valves and actuators is simple as the system does not have to run at all. Even emergency operation is possible in manual mode. But the major benefit for users lies in the newly added KNX communication capability of the SSA actuators. This enables the user application possibilities with room thermostats, as well as room applications with room automation stations or easy connection with control units. The updated SSA actuators reduce the need for wiring and effort, as one and the same cable can be used for communication and power, allowing optimized workflows. Thanks to two digital inputs, window contact, presence detector or condensation sensor c
an be connected, which leads to further wiring reduction, cost savings and also saves inputs/outputs on the controller.
an be connected, which leads to further wiring reduction, cost savings and also saves inputs/outputs on the controller.
This press release and press pictures are available at https://sie.ag/3iVwauK
For more information on Siemens Smart Infrastructure, see www.siemens.com/smart-infrastructure
For further information on the Acvatix portfolio, please see www.siemens.com/Acvatix
For more information on Siemens Smart Infrastructure, see www.siemens.com/smart-infrastructure
For further information on the Acvatix portfolio, please see www.siemens.com/Acvatix
Follow us on Twitter
Siemens Smart Infrastructure (SI) is shaping the market for intelligent, adaptive infrastructure for today and the future. It addresses the pressing challenges of urbanization and climate change by connecting energy systems, buildings and industries. SI provides customers with a comprehensive end-to-end portfolio from a single source – with products, systems, solutions and services from the point of power generation all the way to consumption. With an increasingly digitalized ecosystem, it helps customers thrive and communities progress while contributing toward protecting the planet. SI creates environments that care. Siemens Smart Infrastructure has its global headquarters in Zug, Switzerland, and has around 72,000 employees worldwide.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. Active around the world, the company focuses on intelligent infrastructure for buildings and distributed energy systems and on automation and digitalization in the process and manufacturing industries. Siemens brings together the digital and physical worlds to benefit customers and society. Through Mobility, a leading supplier of intelligent mobility solutions for rail and road transport, Siemens is helping to shape the world market for passenger and freight services. Via its majority stake in the publicly listed company Siemens Healthineers, Siemens is also a world-leading supplier of medical technology and digital health services. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the transmission and generation of electrical power that has been listed on the stock exchange since September 28, 2020.
In fiscal 2020, which ended on September 30, 2020, the Siemens Group generated revenue of €57.1 billion and net income of €4.2 billion. As of September 30, 2020, the company had around 293,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Elisavet-Vasiliki Sachinidou
Siemens S.A.
6-8 Agisilaou Str.
Marousi,P.O. 151 23
Greece
Marousi,P.O. 151 23
Greece
(+30) 210-6864267