Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Premiere at IAA: Walk-in Model shows Munich’s new XXL S-Bahn

Walk-in model of Munich's new XXL S-Bahn

(Munich, September 8, 2025) During IAA Mobility, visitors can step inside the S-Bahn of the future for free at Munich's Königsplatz: The Free State of Bavaria, Deutsche Bahn, and Siemens are presenting a walk-in 1:1 scale model of the new S-Bahn train generation for the first time, which will operate in and around Munich starting in late 2028. At 22 meters in length, the design, equipment, and passenger information of the XXL S-Bahn can be experienced by everyone.
Evelyn Palla, Member of the Management Board for Regional Transport at Deutsche Bahn AG: "This is what the future of public transport looks like: At over 200 meters in length, the new S-Bahn trains offer more space and more comfort. They are designed to allow passengers to board faster, making operations more reliable. Together with the commissioning body and the manufacturer, we are setting the standard for a completely new travel experience. This project shows that mobility of the future can only be shaped together – and that fits perfectly with the IAA, where we as DB are participating precisely under this theme. Because everyday mobility is more than just driving a car."
Dr. Markus Söder, Bavarian Minister President: "Mobility of the Future: The new S-Bahn in white-and-blue Bavaria design will be our most modern S-Bahn. Siemens Mobility has succeeded in creating a real eye-catcher 'Made in Bavaria'. It offers more comfort and more capacity: The approximately 200-meter-long train has space for 1800 passengers and is equipped with state-of-the-art technology and high comfort. Bavaria is growing and growing, which is why we need an efficient public transport system. The Free State has already invested over one billion Euros in the second main line, among other things. In conjunction with the new digital interlocking system at Ostbahnhof, we hope that greater punctuality and reliability will become standard in public transport. Only then can we convince more people to make the switch. After all, one XXL S-Bahn is intended to replace 1500 cars. I wish everyone a good, safe, and punctual journey at all times!"
Christian Bernreiter, Bavaria's Minister of Transport: "The S-Bahn mock-up is a real appetizer for the new era in local mobility around the Bavarian capital. Together with DB and Siemens, something extremely functional and exemplary is growing here. I am particularly pleased that passengers were involved in the development process and can now see how their ideas have been implemented into reality. IAA Mobility is the fitting platform to make this upcoming innovation accessible to passengers, railway enthusiasts, and design lovers for the first time."
Dr. Roland Busch, CEO Siemens AG: "Our new S-Bahn is Munich’s pace-setter for the future: highly reliable in operation, intuitive for staff, and comfortable for every passenger. From virtual design to automated operation, it brings genuine digital intelligence onto the tracks. We made it possible in close collaboration with Deutsche Bahn, the Free State of Bavaria, and S-Bahn München – and through the expertise of our Allach, Erlangen, and Krefeld sites, some of Europe’s most advanced train and R&D centers. With this project, we’re not just kick-starting a greener mobility transition; we’re also delivering on our ‘Made for Germany’ initiative to drive growth and competitiveness in Germany."
Intelligent Design for More Comfort and Reliability
Externally, the S-Bahn logo with a diamond pattern and the colors white and "Bahnland Bayern" blue characterize the design. Inside, yellow accents and natural tones complement the spectrum. With time-dependent lighting, a bright, modern interior is created, equipped with robust and sustainable materials. Greater seat spacing, USB-C sockets, mobile phone signal-permeable windows, Wi-Fi, and a powerful air conditioning system designed for outside temperatures up to 45 degrees Celsius ensure more comfort.
Clearly marked areas for wheelchairs, strollers, and bicycles, along with spacious boarding areas, ensure greater punctuality: Passengers can guide themselves and distribute more quickly with floor markings. The five large multi-purpose areas also contribute to this. Their capacity can adjust flexible using 80 automatically locking folding seats. Modern camera technology helps to ensure that the train can be dispatched more quickly at stations.
New standards in accessibility are set by wide, step-free gangways between carriages and wheelchair spaces with eye-level displays that provide information on elevator status and platform height. Passengers with hearing aids can connect via Bluetooth for announcements. Tactile pictograms, Braille, acoustic signals, and high-contrast design complete the accessibility features.
168 displays make passenger information completely digital for the first time – from the network map and journey progress to the position of elevators and exits at the next platform. Outside, an LED strip in the color of the respective S-Bahn line provides quick orientation on the platform.
For the design, the Free State of Bavaria and DB, together with the design agency Neomind, surveyed passengers, conducted tests, and spoke with politicians, passenger associations, and stakeholder groups. This resulted in a vehicle that optimally combines diverse needs.
State-of-the-Art Technology for More Reliability
The new trains are more innovative, digital, and connected than ever before: A focus is on minimal lifecycle costs through maximum energy efficiency, minimized maintenance costs, and optimized operational support. Thus, the S-Bahn trains have a high number of redundant components and are equipped with the Railigent X system, which ensures the highest availability of the trains. Railigent X is part of the open, digital business platform Siemens Xcelerator, which enables customers to achieve a simpler, faster, and more scalable digital transformation. Furthermore, software updates no longer need to be laboriously installed manually at the depot; instead, they reach the trains during maintenance via a secure online connection.
Siemens Mobility equips all vehicles with Siemens Mobility's European Train Control System (ETCS) and Automatic Train Operation (ATO), as well as a Train Integrity Monitoring System (TIMS). The ETCS of the vehicles combines state-of-the-art, reliable technology, lower maintenance costs through standardization, and brings interoperability to the Munich rail network, which DB plans to digitize and equip with ETCS trackside equipment from 2030. Through the integration of ATO over ETCS, the new S-Bahn trains are ready for the future of rail transport.
Experience the Model at IAA Mobility
The model is located at the IAA Mobility Open Space on Munich's Königsplatz, between the Propylaea and the Glyptothek, directly next to the DB initiative "Future of Local Transport." Interested visitors can view it for free during IAA Mobility from 11 AM to 9 PM (Sunday: 10 AM to 5 PM). The interior is accessible with guided tours, for which you can register on-site. Until the new S-Bahn trains are put into operation, the model will be located near the future S-Bahn depot in Pasing-Langwied. There, it will serve for further tests to ensure a perfectly designed vehicle can be put into service at the end of 2028. 

Press Pictures

Walk-in model of Munich's new XXL S-Bahn

Dr. Roland Busch, CEO Siemens AG / Dr. Markus Söder, Bavarian Minister-President / Christian Bernreiter, Bavaria's Minister of Transport / Evelyn Palla, Member of the Management Board for Regional Transport at Deutsche Bahn AG / Heiko Büttner, Chairman of the Management S-Bahn Munich

Siemens Mobility is a separately managed company of Siemens AG. As a leader in intelligent transport  solutions for more than 175 years, Siemens Mobility is constantly innovating its portfolio. Its core areas  include rolling stock, rail automation and electrification, a comprehensive software portfolio, turnkey  systems as well as related services. With digital products and solutions, and the use of industrial AI,  Siemens Mobility is enabling mobility operators worldwide to make their infrastructure intelligent,  increase value sustainably over the entire lifecycle, enhance passenger experience, and guarantee  availability. In fiscal year 2024, which ended on September 30, 2024, Siemens Mobility posted revenue of  €11.4 billion and employed around 41,900 people worldwide. Further information is available at:  www.siemens.com/mobility
Read more

Контакт

Silke Thomson-Pottebohm

Siemens Mobility

+49 (174) 3063307