Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Bremen orders new tram fleet from Siemens

"Modern, comfortable, reliable, durable and naturally barrier-free – that's the new tram for everyone in Bremen," said of BSAG board spokesman Hajo Müller. "Today's signing of the contract marks a milestone for mass transit in Bremen and the surrounding region. The Avenio is the ideal tram for Bremen's community. With its spacious interior, wireless Internet access and information system with double monitors, it fulfills all the demands for comfort and quality that we and our riders expect of a modern tram."
"Following Munich, The Hague and Doha, Bremen is now the fourth city we are supplying with the Avenio. Our modular design ensures that the Avenio can be tailored to each city's particular needs and can also be flexibly used in a demanding infrastructure," said Jochen Eickholt, CEO of Siemens Mobility.
The Avenio can clearly be identified as a new member of the BSAG fleet: It features the company's signature bright red paint and references to the linear design and the BSAG logo used on earlier trams.
The interior design allows speedy boarding and alighting, shortening stops at the stations. A reflector strip runs along the exterior of the Avenio and is interrupted at the doors. The automatic door openers are marked with striking LED lighting that recalls the BSAG logo and are easy to spot in the dark and by those with impaired eyesight. Riders can quickly and easily move from the entry areas along the level aisle to available seats and standing room throughout the train. The four-section modules form a single, spacious interior. Large windows and LED lighting provide pleasant lighting conditions.
Riders with reduced mobility in wheelchairs or with walkers have spacious areas available at the entrances with convenient seating or room for parking. An electric lift at the second door operates a complete section of the floor. Bicycles and baby strollers can also be parked in the multifunctional areas near the doors. A color-coded guidance system provides additional orientation assistance for visually impaired riders. An air conditioning system ensures a pleasant, draught-free interior atmosphere throughout the year. The tram is up to 90-percent recyclable. The Avenio uses a large part of its recovered braking energy for heating or feeds it back into the power grid. The tram uses energy-saving LED lighting exclusively.

Technical data for Bremen's Avenio:
  • 4-section articulated tram
  • Car body in steel, CDP-coated
  • Gauge: 1,435 mm
  • Vehicle length: ca. 37 m
  • Vehicle width: 2.65 m
  • Capacity: 259 passengers
  • Maximum speed: 70 km/h
  • Maximum axle load: 10.5 metric tons
This press release and additional material are available at: www.siemens.com/press/Avenio-Bremen
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Read more

Contacto

Eva Haupenthal

Siemens AG

Wittelsbacherplatz 2
80333 Munich
Germany

+49 (89) 636-24421