Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release05 June 2018Digital Factory Nuremberg
Universal coupling relays with user-friendly connection and wide-range input
Sirius 3RQ2 from Siemens is a new range of coupling relays with truly universal application scope. With their minimal mounting depth of 90 millimeters and wide-range power supply from 24 to 240 volts AC/DC, these relays are available in variants with between one and three changeover contacts.
With its new, high-grade industrial-duty enclosure in titanium gray design, the new Sirius 3RQ2 coupling relay series blends in visually with the rest of the Sirius relay family. The user-friendly connection methods available offer a range of benefits such as simpler handling, installation, servicing and wiring. Connection is made particularly convenient by the large terminal cross-section of up to four square millimeters and permanent wiring with removable screw-type or spring-type (push-in) terminals. The terminal covers are labeled to simplify wiring assignment, and a DataMatrix code enables easy access to services and support. An extensive array of international standards and certifications such as CE, UL/CSA and EAC makes the new coupling relay ideal for wide-ranging uses including railway applications.
Background information
When standard controllers with standard inputs and outputs reach the limits of their capacity, coupling relays come into their own. They are used for the galvanic isolation of I/Os and PLC inputs and outputs, to amplify and reproduce signals or convert them to different voltage levels and signal forms. Coupling relays and interface converters for different requirements and applications are part of the extensive Sirius industrial controls portfolio from Siemens.
More information is available at www.siemens.com/sirius
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 377,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Gerhard Stauss
Siemens AG
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (911) 895-7945