Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release26 May 2015Joint Press Release by Siemens and SWU Verkehr GmbHMunich/Ulm
Twelve Siemens streetcars for Ulm
Contract signing - Twelve Siemens streetcars for Ulm, Germany
"The Avenio is similar in many ways to the existing Combino with the result that we can offer our passengers a reliable vehicle," stated Ingo Wortmann, managing director of SWU Verkehr, very satisfied with the result of the invitation to tender concluded mid-2014. He added: "This means that we will be able to operate the two future tram lines from an almost standardized vehicle pool. That will also be economically reasonable.
"This order is an important milestone for the streetcar business at Siemens. After Munich, the order from Ulm is the second one we have received from Germany. All eight new trams have been in service in the Bavarian capital since the start of the year," explained Sandra Gott-Karlbauer, CEO of the Urban Transport Business Unit at Siemens. "But at the same time the vehicles for Ulm represent a first too. This is the first time a multi-articulated version of the Avenio is being deployed".
The Ulm metropolitan area is among the fastest growing economic regions in Germany. As a result, it has a commensurate need for mobility in public transportation. The municipal council called on SWU Verkehr GmbH in 2009 to plan a second streetcar line for Ulm. The new Line 2 connects the science district in the north of the city with the central train station, downtown, and Kuhberg to the southwest. The Ulm city council decided on May 6, 2015 with a large majority to go ahead with the construction.
The new streetcar line will have 20 stations and measure 10.5 kilometers long, of which 9.3 kilometers and 18 stations have yet to be built. Construction of the new line and a depot expansion will require an investment of some 192 million euros. Federal and state funds will cover 85.3 million euros of the construction costs. The remainder of the investment will be funded by the City of Ulm. The bus network will also be adapted. This will enable the streetcar to be optimally incorporated into the existing transportation network. The city of Ulm will also designate new residential building areas along the tram line which will provide new impulses in urban development.
A five-car Avenio M will run on the new line in Ulm. The 31 meter long, 100% low-floor light rail vehicle can accommodate up to 175 passengers. A combination of the proven multi-articulated concept with experience gleaned from the Avenio generation makes this possible. The weight-optimized aluminum car body and the already standard Avenio state-of-the-art drive and control technologies minimize energy consumption and save operating costs. The interior of the streetcar is characterized by transparency, giving passengers a feeling of safety and comfort. Amply dimensioned aisles also above the bogies and – in comparison with Combino vehicles – a larger first door improve passenger circulation. During operation, the Avenio M can store and re-use valuable braking energy instead of losing it as heat, which makes a significant contribution to reducing the city's carbon footprint.
As to its appearance, the Avenio has a different front and rear design to the Combino currently operating in Ulm. The new cars will be given the familiar SWU design with the colors blue, light-gray and white. The typical, curved side profile of the power car will be further developed in line with the current Combino design. Another tradition that will be continued: every car will bear the name of a historical figure linked to the city of Ulm.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is No. 1 in offshore wind turbine construction, a leading supplier of combined cycle turbines for power generation, a major provider of power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2014, which ended on September 30, 2014, Siemens generated revenue from continuing operations of €71.9 billion and net income of €5.5 billion. At the end of September 2014, the company had around 343,000 employees worldwide on a continuing basis. Further information is available on the Internet at www.siemens.com.
Contact
Ellen Schramke
Siemens AG
Nonnendammallee 101
13629 Berlin
Germany
13629 Berlin
Germany
+49 (30) 386-22370