[{"name":"Home","site_name":"Press | Company | Siemens","description":"","url_str":"\/global\/","level":0,"image":"","base_root":"https:\/\/press.siemens.com","base_nid":"5","base_nodepath":"\/node\/5","base_path":"\/global\/","base_secure_url":"https:\/\/press.siemens.com\/global","children":null}]
[]
Please use another Browser
It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and
usability.
For the best experience we suggest that you download the newest version of a supported browser:
Press Release07 May 2018,
updated09 May 2018Process Industries and DrivesNuremberg
Transmitter offers high reliability in temperature measurement
Dual sensor operation with 4 wire sensor connection
Automatic redundancy switching for lossless recordings
Wide range of hazardous approvals
Versatile use in chemical, oil and gas, marine and power generation applications
With Sitrans TH320/420 and TR320/420, Siemens introduces a new generation of reliable HART (Highway Addressable Remote Transducer Protocol) temperature transmitters for a wide range of sensor types suitable for mounting in sensor head and rail mounting. They feature high availability of the measurement signal and ease of use. Due to the safety integrity level (SIL) 2/3 certification according to IEC 61508 the temperature transmitters are particularly suited for safety-critical applications. The devices also have a large number of country specific explosion protection certificates for all zones. They provide reliable results even under extreme conditions up to -50°C. Main application areas include industries such as chemical, oil and gas, marine and power generation.
Dual sensor operation with 4 wire sensor connection
Automatic redundancy switching for lossless recordings
Wide range of hazardous approvals
Versatile use in chemical, oil and gas, marine and power generation applications
With Sitrans TH320/420 and TR320/420, Siemens introduces a new generation of reliable HART (Highway Addressable Remote Transducer Protocol) temperature transmitters for a wide range of sensor types suitable for mounting in sensor head and rail mounting. They feature high availability of the measurement signal and ease of use. Due to the safety integrity level (SIL) 2/3 certification according to IEC 61508 the temperature transmitters are particularly suited for safety-critical applications. The devices also have a large number of country specific explosion protection certificates for all zones. They provide reliable results even under extreme conditions up to -50°C. Main application areas include industries such as chemical, oil and gas, marine and power generation.
The image shows a new generation of temperature transmitters.
With fast and accurate sensor and transmitter tuning, the use of the Callendar-van Dusen method or 60-point-curve ensures highest measuring accuracy. Deviations can be detected and monitored through the drift detection with dual-channel transmitters, e. g. for preventive maintenance. Electronic device descriptions (EDD, DTM and FDI) allow the new transmitters to be used in all current distributed control systems. A quick start wizard is just one example of their user-friendly features. Measurement values, device functions and visual alarm signals can be displayed and operation planning and implementation is very convenient using special visualization components for Simatic PCS 7 (Sitrans Library).
When a sensor fails in operation, for example due to disconnection or short circuit, measurement failures may result in loss of control or production stops. To avoid this and ensure high measurement availability through reliability and long term stability, maintenance planning is essential. The Sitrans TH420 and TR420 sensor backup function, drift detection and alarming make this possible. Using the 4 wire connection for both sensors increases data accuracy and reliability as it allows a seamless transition to the second sensor in case the first sensor fails. The continuous balancing of the two independent sensors measuring in parallel, while detecting and monitoring measuring value deviations, allows the scope of maintenance to be planned as required, following the description above, and production stops to be avoided. Balancing the sensors using the Callendar-van Dusen method also meets the challenge of sensor inaccuracy caused by individual deviation from standardized Pt100 curves or by aging. Outstanding transmitter accuracy and sensor balancing enable simpler calibration of the sensors directly in the transmitter and provide for highly precise individual values.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 377,000 employees worldwide. Further information is available on the Internet at www.siemens.com.