Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Siplus HCS4300 and HCS4200: space-saving, high-performance heating solution 

With the new POM4320 Highend power output module for 230/277 and 400/480 V power supply networks, the Siplus HCS4300 heating control system can now control electrical heating elements up to 60 A. Three outputs per module can be used at 60 A, six outputs at 30 A. Integrated current measurement for each output enables heating elements connected in parallel to be monitored so faults can be diagnosed. Three-phase heating elements in a closed triangle, as are typically used in applications with higher power ratings can now also be controlled.
For small heating applications with up to 32 heating elements, the HCS4200 heating control system offers a particularly space-saving solution with the compact CIM4210C central interface module, which is just 104 mm wide. As a result, this HCS solution is also particularly well-suited for use in flat control cabinets. All POMs of the HCS4200 can be used in the two slots of the compact CIM.
The Siplus heating control system can be integrated particularly easily into the automation environment via the engineering framework Totally Integrated Automation Portal (TIA) – with minimal cabling effort and fast commissioning. An HCS program library and user examples simplify engineering even further. Smart control routines ensure that the load is distributed evenly across the network, while integrated diagnostic functions enable faults to be detected and localized rapidly. 
Heating control systems from Siemens can be found in a range of sectors and applications all over the world: for example, in the drying of paint and coatings, in the molding of plastics and lightweight construction materials, in plastic welding, and in infrared oven baking.
Additional Information can be found at
www.siemens.com/siplus-hcs
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 76,000 employees internationally.
Read more
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of power generation and distribution, intelligent infrastructure for buildings and distributed energy systems, and automation and digitalization in the process and manufacturing industries. Through the separately managed company Siemens Mobility, a leading supplier of smart mobility solutions for rail and road transport, Siemens is shaping the world market for passenger and freight services. Due to its majority stakes in the publicly listed companies Siemens Healthineers AG and Siemens Gamesa Renewable Energy, Siemens is also a world-leading supplier of medical technology and digital healthcare services as well as environmentally friendly solutions for onshore and offshore wind power generation. In fiscal 2019, which ended on September 30, 2019, Siemens generated revenue of €86.8 billion and net income of €5.6 billion. At the end of September 2019, the company had around 385,000 employees worldwide. Further information is available on the Internet at www.siemens.com .
Read more

Contact

Andreas Friedrich

Digital Industries

+49 1522 2103967