Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release24 April 2017Process Industries and DrivesNuremberg
Sinacon HC – hybrid converter for innovative grids
The picture shows the hybrid converter Sinacon HC by Siemens.
This modular, flexible hybrid converter concept works in conjunction with different decoupled DC sources. This allows different sources of energy, for instance, to be connected to the grid using just a single converter with different DC and AC terminals. The wide voltage range from 100 to 1150 Volts (V) DC allows an extensive choice of different batteries to be connected independently of the AC mains voltage level. This makes the converter compatible with all kinds of different batteries, from lithium ion through redox flow batteries or fuel cells. The AC voltage of 620 V allows the creation of standardized solutions and opens up potential for savings in the system. The broad scope of the converter opens up new business fields, both as a grid support and also for the creation of microgrids through the use of renewables combined with battery storage systems. The common inverter allows new concepts to be implemented and operated with the greatest of ease, for instance the use of renewable energy sources in combination with grid support, or the implementation of renewable energy in microgrids to save fuel costs. A consistently high grid quality is assured throughout by an optimized grid filter concept with hysteresis current control.
The hybrid converter comes with all the necessary conditions for feeding into medium-voltage grids, and is certified for local power grid standards (such as BDEW, UL1741, TAB HV).
The type tested, ready-to-connect cabinet system combines reliability with outstanding availability and efficient support through the global Siemens service platform. It also offers extensive scope for remote maintenance, control and operating status diagnosis using a web server.
For further information on topic Sinacon HC, please see www.siemens.com/sinacon-hc
For further information on Siemens at the Hannover Messe 2017, please see www.siemens.com/press/hm17 and www.siemens.com/hannovermesse
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Stefan Rauscher
Siemens AG
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (911) 895-7952