Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release27 March 2023Digital IndustriesNuremberg
Siemens Xcelerator: New Sinamics G220 high-performance frequency converter for greater efficiency, easier engineering and faster comissioning

The new Sinamics G220 frequency converters are the first Sinamics drives to be part of the Siemens Xcelerator portfolio.
As a result, the Sinamics G220 frequency converters are significantly more efficient in terms of space utilization and operation and make engineering much easier.The new frequency converters
are also the first Sinamics drives to be part of the Siemens Xcelerator
portfolio, the Siemens-wide business platform for digital transformation. This
is because Sinamics G220 frequency converters are also an integral part of the
TIA portal and have a digital twin in Startdrive, the commissioning tool for
drives. This allows the behavior of the drive to be tested and optimized before
the hardware is available. With the integrated web server, commissioning times
can also be significantly reduced. The new converters are also equipped with an
IIoT module. This means that Sinamics G220 frequency converters can be easily
integrated into cloud and edge applications, which increases the transparency
of their applications. Availabilities can thus be optimized, and downtimes avoided. In the area of cybersecurity, the Sinamics G220 is equipped with Security Integrated as standard, providing secure communication, integrity and authenticity checks to protect against tampered firmware, and User Management & Access Control.
Sinamics G220 converters come with a range of
hardware options and software functions, allowing them to be flexibly adapted
to the respective application cases required. For example, the Sinamics G220 is
also available in IP55 and there are special coatings for harsh environments.
Thanks to the high-quality components and hardware design, the drive is
designed for a long service life. When it comes to Safety Integrated, the new
frequency converters reach the next level by meeting SIL 3 requirements.
Sinamics G220 are suitable for all industries, but especially for the food
& beverage, pharmaceutical, chemical, oil & gas, and marine industries.
Further
information on Siemens at Hannover Messe 2023 at
www.siemens.com/press/hm23 and www.siemens.com/hannover-messe
www.siemens.com/press/hm23 and www.siemens.com/hannover-messe
For this press release
Follow us on our social media channels
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 76,000 employees internationally.
Siemens AG (Berlin and Munich) is a technology company focused on industry, infrastructure, transport, and healthcare. From more resource-efficient factories, resilient supply chains, and smarter buildings and grids, to cleaner and more comfortable transportation as well as advanced healthcare, the company creates technology with purpose adding real value for customers. By combining the real and the digital worlds, Siemens empowers its customers to transform their industries and markets, helping them to transform the everyday for billions of people. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a globally leading medical technology provider shaping the future of healthcare. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the transmission and generation of electrical power.
In fiscal 2022, which ended on September 30, 2022, the Siemens Group generated revenue of €72.0 billion and net income of €4.4 billion. As of September 30, 2022, the company had around 311,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
In fiscal 2022, which ended on September 30, 2022, the Siemens Group generated revenue of €72.0 billion and net income of €4.4 billion. As of September 30, 2022, the company had around 311,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Reference Number: HQDIPR202303246666EN