Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Siemens Xcelerator: DMG MORI, Renishaw, and Siemens are working as innovation partners and expanding digital offerings for machine tools

Renishaw: Quality monitoring of tools at the highest level

The Siemens Xcelerator offering from Renishaw consists of a solution for measuring and monitoring the condition of tools. The basic system is already offered by DMG MORI. The solution is based on a high-precision laser system for tool measurement from Renishaw and the edge-based analysis software Analyze MyWorkpiece /Monitor from Siemens. The condition monitoring solution enables the automatic validation of tool wear and the timely automatic replacement of worn tools. The solution also ensures that the manufacturing process is traceable thanks to data evaluation. The fast tool inspection by optical scanning reduces manual intervention and therefore disruptions within the manufacturing process. The data-driven analysis approach ensures the traceability of the manufacturing process, which closes the loop in terms of quality assurance and production planning (closed-loop manufacturing). At AMB, the solution will be on display for the first time at DMG MORI (Hall 10) and at Renishaw (Hall 7, booth A11) on a DMU 60 eVo.

DMG MORI: Scalable offering for the end-to-end digital twin for machine tool machining at the Siemens Xcelerator Marketplace

The manufacturer of high-precision machine tools, DMG MORI, is expanding its offering for the end-to-end digital twin for machine tool machining on the Siemens Xcelerator Marketplace. Specific solutions for the digital twin of the control system, machine, and workpiece will be presented for a variety of applications. This makes it possible to optimize machining processes long before the real machine is put into operation. Based on the digital native CNC Sinumerik One, the portfolio includes a tailored digital twin for the user – regardless of the shop floor or CAM applications. For example, machine operators on the shop floor can purchase a digital twin package that allows them to create a simple NC program on the PC and thus carry out a collision check without using the machine. A CAM user, on the other hand, can create sophisticated parts in a CAD environment and perform a quick initial validation of the program. With DMG MORI’s new, scalable digital twin offerings, customers can now individually determine the scope of the required simulation and purchase the corresponding packages.
The DMG MORI digital twin for machine tool machining helps to avoid programming errors that cause rejects and damage to the actual machine. It can ramp up production up to 40 percent faster, significantly reducing the energy consumption of the real machine. Even new processes can be set up digitally while the machine is in operation. It also helps to reduce unproductive machine times, such as test machining, by as much as 75 percent. This is because the testing and running-in of programs is transferred from the actual machine to the virtual world.
The DMG MORI machines DMU 50 3. Generation, CTX beta 450 TC, and NZ TRE rely on the Sinumerik One with its performance and state-of-the-art shop floor programming. At the trade fair, visitors can experience the machines and their end-to-end digital twin first-hand at the DMG MORI booth in Hall 10.
The Siemens Xcelerator offering from Renishaw consists of a solution for measuring and monitoring the condition of tools.
With the new, scalable digital twin offerings from DMG MORI, customers can now individually determine the scope of the required simulation and purchase the corresponding packages.
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions, and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has employed around 72,000 people internationally.
Read more
Siemens AG (Berlin and Munich) is a leading technology company focused on industry, infrastructure, transport, and healthcare. From more resource-efficient factories, resilient supply chains, and smarter buildings and grids, to cleaner and more comfortable transportation as well as advanced healthcare, the company creates technology with purpose adding real value for customers. By combining the real and the digital worlds, Siemens empowers its customers to transform their industries and markets, helping them to transform the everyday for billions of people. In fiscal 2023, which ended on September 30, 2023, the Siemens Group generated revenue of €77.8 billion and net income of €8.5 billion. As of September 30, 2023, the company employed around 320,000 people worldwide. Further information is available on the Internet at www.siemens.com.
Read more
Reference Number: HQDIPR202409056991EN

Contact

Katharina Rebbereh

Siemens AG

+49 172 841 35 39