Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release18 December 2014Joint press release Siemens, Stadtwerke AugsburgMunich
Siemens to use superconductors in building the power grid of the future in Augsburg
Siemens to use superconductors in building the power grid of the future in Augsburg
Superconducting fault current limiters can limit short-circuit currents in power transmission and distribution grids very quickly, effectively, automatically and, thus, with a high degree of intrinsic safety, making reliable grid operation possible even under difficult conditions. After a short cooling period, the grids can also return to normal operation without additional measures.
"With our innovative partner, Stadtwerke Augsburg, we have a power utility where we can demonstrate how this advanced technology can help master the challenges of the energy transition and grid upgrades successfully," said Dr. Tabea Arndt, head of Superconducting Components and Applications at Siemens Corporate Technology. "Powerful plants for renewable energies (EEG plants) must be connected to the grid via efficient fault current limiters to protect the electric components," said Jürgen Völkel, technical director of Stadtwerke Augsburg. Project head Thomas Janetschek added, "We already know where these could potentially be installed immediately."
Superconducting fault current limiters also have another advantage: they are "invisible" for the grid in normal operation since they have no electrical resistance at their low operating temperature of -196o Celsius. As a result, the limiters do not negatively impact the power grid's stability – unlike today's conventional short-circuit limiting reactors that have a continuously high resistance. On average, about 25 kilowatts of electricity is lost per conventional limiting reactor.
Superconducting fault current limiters also make it possible to link several different power sub-grids, thereby increasing operational security and grid stability. In addition, using the limiters to link several sub-grids or to connect decentralized energy feeders eliminates the added costs of replacing or upgrading electrical components that are frequently incurred when power grids are strengthened.
For this press release
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is No. 1 in offshore wind turbine construction, a leading supplier of combined cycle turbines for power generation, a major provider of power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2014, which ended on September 30, 2014, Siemens generated revenue from continuing operations of €71.9 billion and net income of €5.5 billion. At the end of September 2014, the company had around 357,000 employees worldwide. Further information is available on the Internet at http://www.siemens.com.
Stadtwerke Augsburg is the third largest multi utility company in Bavaria, Germany. In the Augsburg region it supplies over 350,000 people with energy and drinking water and guarantees easy mobility with modern means of transport. As a hundred-percent municipal company it contributes substantially to the efficiency of the city of Augsburg. Further information can be found on the Internet at www.sw-augsburg.de.
Stadtwerke Augsburg is the third largest multi utility company in Bavaria, Germany. In the Augsburg region it supplies over 350,000 people with energy and drinking water and guarantees easy mobility with modern means of transport. As a hundred-percent municipal company it contributes substantially to the efficiency of the city of Augsburg. Further information can be found on the Internet at www.sw-augsburg.de.
Contact
Harald Hassenmüller
Siemens AG
Wittelsbacherplatz 2
80333 Munich
Germany
80333 Munich
Germany
+49 (89) 636-32187