Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release21 October 2024Smart InfrastructureZug, Switzerland
Siemens unveils innovative motor management system for industrial switchboards

SIMOCODE M-CP
Space-saving and flexible installation
The new SIMOCODE M-CP is optimized for withdrawable units in
switchboards. With the ability to choose between front panel mounting and
mounting on a DIN rail, this versatile device allows for optimizing space and
reducing installation expense. More integrated functions in the basic unit
ensure less variance. Six digital inputs and four relay outputs eliminate the
need for additional modules.
Advanced communication with Single Pair Ethernet
To enable fast and reliable data transmission, SIMOCODE M-CP
uses Single Pair Ethernet (SPE) technology. This new bus physics ensures
uninterrupted Ethernet communication and fulfills the needs of switchboard
operations, while reducing wiring complexity with its thin, two-core cables.
Communication in the withdrawable unit is enabled via just two wires.
Future-proof technology with reloadable and licensable functions
In the future, SIMOCODE M-CP can be adapted to different
operational requirements by purchasing licenses that enable additional
functions depending on the application. This reduces the need for purchasing
and installing separate products and makes the system future-proof. One example
is the integration of condition monitoring directly into the motor management
system. This eliminates the need for separate sensors. Key parameters can now
be monitored using the motor along with current and voltage measurement
modules, simplifying the setup. By purchasing a license, users can activate the
provision of data through SIMOCODE M-CP for advanced features for motor current
signature analyses (MCSA) or the employment of AI for detecting anomalies and
damages in motors and machines, streamlining the process and improving
reliability.

SIMOCODE M-CP in the withdrawable unit
Built-in sustainability
Besides using recycled materials for production and
packaging, the high quality of the products pays off with a long service
life.
With its multitude of diagnostic functions, SIMOCODE M-CP can
help increase system availability and extend the service life of motors by
providing early warnings in the event of irregularities. Long-term firmware
updates also help ensure that SIMOCODE M-CP remains functional and up to date
for years to come.
For this press release
Follow us on X
Siemens Smart Infrastructure (SI) is shaping the market for intelligent, adaptive infrastructure for today and the future. It addresses the pressing challenges of urbanization and climate change by connecting energy systems, buildings, and industries. SI provides customers with a comprehensive end-to-end portfolio from a single source – with products, systems, solutions, and services from the point of power generation all the way to consumption. With an increasingly digitalized ecosystem, it helps customers thrive and communities progress while contributing toward protecting the planet. Siemens Smart Infrastructure has its global headquarters in Zug, Switzerland. As of September 30, 2023, the business had around 75,000 employees worldwide.
Siemens AG (Berlin and Munich) is a leading technology company focused on industry, infrastructure, mobility, and healthcare. The company’s purpose is to create technology to transform the everyday, for everyone. By combining the real and the digital worlds, Siemens empowers customers to accelerate their digital and sustainability transformations, making factories more efficient, cities more livable, and transportation more sustainable. Siemens also owns a majority stake in the publicly listed company, Siemens Healthineers, a leading global medical technology provider shaping the future of healthcare.
In fiscal 2023, which ended on September 30, 2023, the Siemens Group generated revenue of €74.9 billion and net income of €8.5 billion. As of September 30, 2023, the company employed around 305,000 people worldwide on the basis of continuing operations. Further information is available on the Internet at
www.siemens.com.
Contact
Christian S. Wilson
Siemens Smart Infrastructure
+49 172 138 5608