Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release04 July 2017Building TechnologiesZug
Siemens turns Dubai Opera into a smart concert space
An innovative feature of Dubai Opera is the ability to switch between three usage modes: from a theater to a concert hall to a "flat-floor" mode, which automatically folds away seating to allow the space to be used as a banquet or event hall. The Siemens technology is able to automatically switch the cooling logic of the air conditioning system to maximum visitor comfort and energy efficiency.
The day-to-day operations of the iconic building are monitored and controlled by Siemens' most advanced building management platform, Desigo CC. The intelligent system generates significant resource savings by integrating the management of energy, air conditioning, ventilation and water consumption into a fully customized, graphical 3D interface. Desigo CC also integrates 14 additional subsystems, including access control, video surveillance, lighting control, elevators and escalators, the emergency central battery system and an uninterrupted power supply, giving operators total control over Dubai Opera's operating performance. Typically, Desigo CC achieves reductions in operating costs of up to 20 percent; when combined with other Siemens technologies such as Demand Flow for district cooling, energy savings can reach up to 40 percent.
"Dubai Opera is an important architectural landmark, and embracing the most modern digital technology for building management is a key part of Dubai's drive to become a smart city," said Koen Bogers, Senior Executive Vice President, Building Technologies Division, Siemens Middle East.
With digitalized infrastructure increasingly important as a cornerstone of an energy-efficient smart city, advanced building technology from Siemens has been installed across the Middle East. Recently, Siemens announced that its Desigo building management technology had been implemented at Dubai Parks and Resorts, the Middle East's largest theme park destination. Previous installations include Abu Dhabi's Sheikh Zayed Grand Mosque, Tornado Tower in Qatar, Atlantis Hotel in Dubai and the 3D-printed Office of the Future in Dubai.
For more information about the Building Technologies Division, please visit www.siemens.com/buildingtechnologies.
Siemens AG (Berlin and Munich) ist ein führender internationaler Technologiekonzern, der seit mehr als 165 Jahren für technische Leistungsfähigkeit, Innovation, Qualität, Zuverlässigkeit und Internationalität steht. Das Unternehmen ist in mehr als 200 Ländern aktiv, und zwar schwerpunktmäßig auf den Gebieten Elektrifizierung, Automatisierung und Digitalisierung. Siemens ist weltweit einer der größten Hersteller energieeffizienter ressourcenschonender Technologien. Das Unternehmen ist einer der führenden Anbieter effizienter Energieerzeugungs- und Energieübertragungslösungen, Pionier bei Infrastrukturlösungen sowie bei Automatisierungs-, Antriebs- und Softwarelösungen für die Industrie. Darüber hinaus ist das Unternehmen ein führender Anbieter bildgebender medizinischer Geräte wie Computertomographen und Magnetresonanztomographen sowie in der Labordiagnostik und klinischer IT. Im Geschäftsjahr 2016, das am 30. September 2016 endete, erzielte Siemens einen Umsatz von 79,6 Milliarden Euro und einen Gewinn nach Steuern von 5,6 Milliarden Euro. Ende September 2016 hatte das Unternehmen weltweit rund 351.000 Beschäftigte. Weitere Informationen finden Sie im Internet unter www.siemens.com.
Contact
Catharina Bujnoch-Gross
Siemens AG
Gubelstrasse 22
CH-6301 Zug
Switzerland
CH-6301 Zug
Switzerland
+41 (79) 5660778