Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release14 March 2017Digital Factory Nuremberg
Siemens TIA Portal with more openness and end-to-end work processes

Siemens TIA Portal with more openness and end-to-end work processes.
The TIA Portal engineering framework is a central access point for Siemens when it comes to automation within digital enterprises and the design of automation solutions in the context of digitization. TIA Portal V14 SP1 has also expanded TIA Portal Openness, meaning that it is now easier to make work processes digital from start to finish. For example, the virtual controller Simatic S7-PLCSIM Advanced can be used to test controller functions at an early stage and link them to simulated machine models for virtual commissioning.
Another example is the ability to use Simatic know-how to program and diagnose robot controllers via Simatic S7-1500 function blocks.
From V14 SP1 and V13 SP2 onwards, the TIA Portal engineering framework also supports Windows 10, thus providing flexible coverage for user operating system requirements. To enable the simple and central management of passwords for know-how, write and copy protection, users can take advantage of the all-new password API in TIA Portal V14 SP1. The interface allows the simple implementation of a password management system for proprietary applications or secure authentication concepts using dongles, for example. Simatic ProDiag, the software option for machine and plant diagnostics, has been expanded include criteria analysis for focused troubleshooting. This enables the use of the HMI PLC Code Viewer to retrospectively visualize the states in which faults occurred and to identify their root cause even more efficiently. In the Step 7 engineering tool, machine manufacturers can now use the novel single block comparison function for faster editing, allowing, for example, the detailed comparison of individual blocks directly from the project navigation area in both offline/offline or online/offline operation.
Background information:
The Siemens TIA Portal (Totally Integrated Automation Portal) enables users to perform automation and drive tasks quickly and intuitively through efficient configuration. The software architecture is designed for high efficiency and ease of use, and is suitable for both new and experienced users. It offers a standardized operating concept for controllers, human machine interfaces (HMI) and drives, as well as for shared data storage and consistency, for example during configuration, communication and diagnostics, as well as offering powerful libraries for all automation objects. The simple engineering in the TIA Portal facilitates full access to the entire spectrum of digitized automation, including digital planning, integrated engineering and transparent operation. Alongside PLM (Product Lifecycle Management) and MES (Manufacturing Execution Systems) within the Digital Enterprise Software Suite, the TIA Portal complements the holistic range of software available from Siemens for companies on the path toward Industry 4.0.
Further information about converting can be found at www.siemens.com/tia-portal
For further information on Siemens at the Hannover Messe 2017, please see www.siemens.com/press/hm17 and www.siemens.com/hannovermesse
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Reference Number: PR2017030195DFEN
Contact
Gerhard Stauss
Siemens AG
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (911) 895-7945