Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Siemens supporting Brasília's stadium in bid to become world's greenest sports arena

Green technologies from Siemens can reduce waste at the stadium by controlling water and energy consumption. By helping make Mané Garrincha even more sustainable, the systems will also support the stadium in its bid to become the world's first sports arena to receive LEED Platinum sustainability certification, a status achieved only by buildings meeting the highest environmental standards. The Siemens building automation software installed in the stadium meets the requirements of LEED certification, since it controls the consumption, metering and utilization of water and power, the use of air conditioning and the integration of fire detection, alarm and security systems.
"Siemens' technologies and solutions are now installed in one of the world's most modern stadiums. Participating in the construction of Mané Garrincha National Stadium in Brasília is a source of great pride for us since the project will be an important legacy to Brazil's federal capital," said Guilherme Mendonça, head of the Infrastructure & Cities (IC) Sector in Brazil.
The agreement concluded with the Brasília 2014 Consortium, which comprises the construction companies Andrade Gutierrez and Via Engenharia, provides for the supply of more than 400 CCTV cameras, 150 turnstiles for controlling access at some 6,000 control points and approximately 6,000 fire detection points.
In addition to building automation technologies, the project includes IT and sound systems provided together with partners for the stadium, which, with a seating capacity of 70,000, is Brazil's second-largest sports arena. These technologies and solutions are already a feature of Europe's most advanced and profitable sports facilities, such as the Allianz Arena in Munich, Germany.

Leading-edge technology guarantees greater security
Utilizing state-of-the-art camera technology, the CCTV system supplied by Siemens can identify spectators throughout the stadium's stands. The system, which is managed by high processing capacity software, provides for hierarchical access via password, so that the stadium's security organizations (police, fire brigade and private security) can identify possible problems and take appropriate action.
By integrating the database with the most diverse ticket sale systems, the access control system will enable the facility's operators to promote a wide variety of events. The turnstiles at the arena's entry points will be able to read all currently available identification technologies such as 1D and 2D barcodes, mifare and smartcards. The system's data will be fully encrypted, making operations even more secure and preventing ticket forgery. The system will also protect the technical areas at the stadium, and operators will not need to carry keys to open the numerous stadium gates.
All the technologies supplied will be integrated into the command and control center. This will make it possible to access the stadium's systems and operate them by means of a single screen. Siemens' solutions have already been installed at more than 150 sports facilities worldwide – including the Allianz Arena in Germany, the Gdansk Stadium in Poland and eight arenas in South Africa.

Further information on Siemens technologies for the upcoming major events in Brazil and press pictures are available at www.siemens.com/press/brazil
Follow us on Twitter at: www.twitter.com/siemens_press
Siemens AG (Berlin and Munich) is a global powerhouse in electronics and electrical engineering, operating in the fields of industry, energy and healthcare as well as providing infrastructure solutions, primarily for cities and metropolitan areas. For over 165 years, Siemens has stood for technological excellence, innovation, quality, reliability and internationality. The company is the world's largest provider of environmental technologies. Around 40 percent of its total revenue stems from green products and solutions. In fiscal 2012, which ended on September 30, 2012, revenue from continuing operations totaled €78.5 billion and income from continuing operations €4.7 billion (incl. IAS 19R and reclassification of the solar business into continuing operations). At the end of September 2012, Siemens had around 370,000 employees worldwide on the basis of continuing operations. Further information is available on the Internet at: http://www.siemens.com.
Read more

Contact

Alexander Becker

Siemens AG

Wittelsbacherplatz 2
80333 Munich
Germany

+49 (89) 636-36558