Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release17 January 2019Power and GasHouston
Siemens to supply industrial gas turbines for gas processing facility in Alberta, Canada
The picture shows a SGT-300 gas turbine.
The picture shows a SGT-300 gas turbine.
The gas processing plant will help support production growth for the customer in the Grande Prairie Region, located northeast of Edmonton, and will be built alongside the company's existing dehydration and compression facility. When completed in 2020, the plant will provide the customer with an additional 50 million cubic feet per day of natural gas processing capacity and 30,000 barrels per day of condensate stabilization capacity.
The two SGT-300 industrial gas turbines, which will share 12 megawatts of power generation, met all project requirements and will be used to drive compressors at the facility. The SGT-300 is a robust, proven gas turbine used in power generation and mechanical drive applications throughout the world. It's most renowned for its use in the oil and gas industry, offering a compact arrangement, easy on-site maintainability, and reliability.
The turbine package for the gas plant will feature a non-enclosed design, allowing the plant-wide fire detection and suppression system to ensure worker safety throughout the facility. It will also provide open access for maintenance and visual inspections.
"The SGT-300 unit was a logical choice for this project, given its high efficiency, innovative dry low emissions combustion system, and more than 4.5 million hours of operating experience worldwide," said Matthew Chinn, Executive Vice President of New Equipment Solutions Worldwide for Siemens. "These features will ultimately minimize operational and maintenance costs for the customer over the life of the plant."
The two SGT-300 units are expected to be delivered in late summer 2019, just 10 months after the initial order was placed. Commissioning is expected in autumn 2019.
"Siemens gas turbines continue to be a preferred choice for a wide range of oil and gas applications across northwest Canada," said Patrice Laporte, Vice President of Oil and Gas for Siemens America. "This will be the first application of the SGT-300 in the country and we look forward to working with the customer and their EPC to support future production growth throughout the Grande Prairie Region."
For this press release
@Siemens_Energy
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Janet Ofano
Siemens AG
5101 Westinghouse Boulevard
28273-9640 Charlotte, NC
USA
28273-9640 Charlotte, NC
USA
+1 (803) 389-6753