Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Siemens sets new standards in drive technology with Sinamics S220 drive system

Multi-Axis Control Unit CU320-3: The Technological Heart

At the core of Sinamics S220, the newly developed control unit CU320-3 sets pioneering standards in drive technology with its unique architecture. With the ability to operate up to 12 axes on a single control unit, the system achieves an outstanding level of integration density. The built-in multicore processor provides the necessary computing power, while the Drive-Cliq-Express interface, with a speed of 1GBit/s, ensures rapid data transfer. An innovative test pulse method using three voltage sensors per axis enables sensorless control with near-encoder quality – while also improving energy efficiency and robustness.

Digitalization and Future-Readiness

Sinamics S220 has been fundamentally reconceived to meet the demands of digital transformation. The targeted generation of high-quality field data opens up new business models in Industry 4.0. High-frequency data transmission for predictive maintenance occurs via the X128 interface. Integration into the TIA Portal, as well as virtual commissioning with DriveSim Designer, significantly improve the engineering workflow. New assistants and an undo function facilitate operation. The Smart Drive Interface is available as a compact panel (SDI S220) directly on the CU320-3 or as a remote version (SDI Pro with a larger display and web server). Optionally, a Smart WiFi adapter enables flexible remote access.

Flexibility and scalability

The Sinamics S220 drive system offers a broad performance spectrum for industrial applications. Upon market launch, air-cooled motor modules in booksize and chassis designs, with a voltage range of 3AC 380 to 480 V, are available. The rated current ranges from 3 A (1.1 kW) to 1.518 A (900 kW) and can be expanded up to 6.984 kW through 8-fold parallel connection. For power supply, regenerative active infeeds ranging from 210 kW to 921 kW are available, also scalable through parallel connection. Additionally, air-cooled universal modules are introduced, which can be flexibly operated as motor modules or active line modules. Six devices cover the entire functional and performance range for spare parts cases and allow rapid adaptation to changing requirements.

Safety integrated and cybersecurity at the highest level

With software version 6.6, the Sinamics S220 sets new standards in plant safety. The new safety architecture reduces the safety cycle from 12 ms to 4 ms, enabling faster reactions and higher productivity. Automatic background tests ensure uninterrupted operation, while offline parameterizable safety functions greatly simplify engineering. The drive is SIL 3 certified for all operating states and offers the certified level of safety in critical applications. The Sinamics S220 was developed within a secure development process according to the standard IEC 62443-4-1, independently certified by TÜV SÜD. The drive system features numerous integrated safety functions, including user and access control, encrypted drive data, and integrity and authentication checks for firmware and configuration data. These features, along with additional measures within the machine, enhance resilience against cybersecurity risks.

Sustainable Drive System for the Future of Industry

With Sinamics S220, Siemens presents a drive system that combines sustainability and performance. Its compact design saves space while resource-saving materials and high reparability and recyclability contribute to reducing carbon impact. Industrial Edge applications enable the capture and visualization of energy consumption and CO₂ emissions. The ISO 14021 certified Environmental Product Declaration (EPD) documents its environmental performance over the entire lifecycle, underscoring Siemens’ commitment to sustainable industrial solutions.

For this press release

Press Folders

Follow us on social media

Siemens Digital Industries (DI) empowers companies of all sizes within the process and discrete manufacturing industries to accelerate their digital and sustainability transformation across the entire value chain. Siemens’ cutting-edge automation and software portfolio revolutionizes the design, realization and optimization of products and production. And with Siemens Xcelerator – the open digital business platform – this process is made even easier, faster, and scalable. Together with our partners and ecosystem, Siemens Digital Industries enables customers to become a sustainable Digital Enterprise. Siemens Digital Industries has a workforce of around 70,000 people worldwide.
Read more
Siemens AG (Berlin and Munich) is a leading technology company focused on industry, infrastructure, mobility, and healthcare. The company’s purpose is to create technology to transform the everyday, for everyone. By combining the real and the digital worlds, Siemens empowers customers to accelerate their digital and sustainability transformations, making factories more efficient, cities more livable, and transportation more sustainable. A leader in industrial AI, Siemens leverages its deep domain know-how to apply AI – including generative AI – to real-world applications, making AI accessible and impactful for customers across diverse industries. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a leading global medical technology provider pioneering breakthroughs in healthcare. For everyone. Everywhere. Sustainably. In fiscal 2024, which ended on September 30, 2024, the Siemens Group generated revenue of €75.9 billion and net income of €9.0 billion. As of September 30, 2024, the company employed around 312,000 people worldwide on the basis of continuing operations. Further information is available on the Internet at www.siemens.com.
Read more

Contact

Katharina Rebbereh

Siemens AG

+49 172 841 35 39