Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release23 February 2016Joint Press Release by Siemens, Arriyadh Development Authority and Riyadh MetroMunich
Siemens presents new metro for Riyadh
"Our project teams in Vienna and Saudi Arabia poured all their heart and soul into the development and completion of the first train which is specially equipped for the extreme climatic conditions in Riyadh. So we are especially proud to be the first of the three consortia to present our vehicle to the public," says Jochen Eickholt, CEO of Siemens Mobility. The first train is currently being tested for extreme conditions in the climatic wind tunnel at Rail Tec Arsenal (RTA) in Vienna. In spring 2016, dynamic testing will commence at the Siemens Test and Validation Center in Wildenrath, Germany.
Siemens is to supply 67 Inspiro type metro trains. These trains with their all-aluminum car bodies are designed to run on standard-gauge track at a top speed of 90 km/h. The 2 and 4-car train configurations have been designed with the region's climate in mind. One such feature is a more powerful air conditioning system, capable of delivering sufficient cooling capacity even in extreme heat. In addition, the bogies, traction drive, brakes and doors have been fitted with special elements in order to prevent the ingress of sand.
Siemens is also responsible for integration of the railway systems on these two lines, which cover a total of 64 route kilometers. This investment in the city's infrastructure is meant to alleviate the local traffic problems. A fast growing city, the population of Riyadh has doubled to more than six million people since 1990.
This press release and press pictures are available at www.siemens.com/press/riyadh, www.riyadh-metro.com and www.arriyadh.com
For this press release
Update
This press release was updated on 20.12.2016 at 02:30 PM CET.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is No. 1 in offshore wind turbine construction, a leading supplier of gas and steam turbines for power generation, a major provider of power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2015, which ended on September 30, 2015, Siemens generated revenue of €75.6 billion and net income of €7.4 billion. At the end of September 2015, the company had around 348,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Katharina Zoefeld
Siemens AG
Otto-Hahn-Ring 6
81739 Munich
Germany
81739 Munich
Germany
+49 (89) 636-636802