Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Siemens optimizes converting machines with new compensation functions

Winding on non-circular cylindrical, near elliptical bodies creates web length changes between the material support point and the deflector roller. These were previously compensated mechanically or by a variable winding speed. The new Siemens Motion Control solution for prismatic winding calculates cyclically in advance the support points of the material on the deflector roller and winding body, and feeds these into the controller. The machine constructor benefits from higher winding quality, higher machine speed and process reliability.
The new self-learning LECo application replaces the previous dynamic position controllers. These correct position errors of the process axes caused, for example, by a mechanical shock, but only after a delay. By continuously monitoring the process axes, the new Siemens solution quickly detects deviations, calculates the pre-control value on the basis of the following error, and feeds this into the controller in the next cycle. Deviations are already largely compensated for after the first cycle. In the following cycles, a learning algorithm continuously monitors the result of the compensation, fine tunes the drive control, and thus also increases the process accuracy.

Further information about converting can be found at www.siemens.com/converting
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world’s largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Read more
Reference Number: PR2017030179DFEN

Contact

Gerhard Stauss

Siemens AG

Gleiwitzer Str. 555
90475 Nuremberg
Germany

+49 (911) 895-7945