Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Siemens Mobility to supply first battery powered Mireo Plus B trains to Denmark

“The battery trains are expected to enter service at the end of 2024. This is a crucial step in our own green transition, but also a significant step towards the goal of CO2- neutral train traffic throughout Denmark,” said Martha Vrist CEO Midtjyske Jernbaner Drift A/S.
“With the acquisition of the Mireo Plus B trains, Midtjyske Jernbaner replaces conventional diesel vehicles with state-of-the-art, and locally, completely emissionfree trains. This will significantly contribute to the local area by offering a sustainable and environmentally friendly mobility option. We are delighted that Midtjyske Jernbaner has chosen the energy-efficient Mireo Plus B trains from Siemens Mobility, which will also offer a high level of driving comfort and an improved passenger experience,” said Albrecht Neumann, CEO Rolling Stock at Siemens Mobility.
The Mireo Plus B two-car trainsets can accommodate 120 seated passengers, travel up to 140 km/h and has a range of around 80 kilometers when in battery operation. The batteries can be charged via the 25 kV overhead line in electrified sections and by recuperating the train’s braking energy. The battery system is mounted underfloor and is installed in two battery containers. Lithium-ion batteries with a long service life are used in this system.
This is the third order Siemens Mobility has received for the Mireo Plus B and the first outside of Germany. The Landesanstalt Schienenfahrzeuge Baden-Württemberg (SFBW) ordered 20 Mireo Plus B trains in 2020 and Niederbarnimer Eisenbahn (NEB) ordered 31 in 2021. This technology has been extensively tested for over one year through a preliminary version on a prototype train, the Desiro ML ÖBB Cityjet eco in Austria.

For this press release

Siemens Mobility is a separately managed company of Siemens AG. As a leader in transport solutions for more than 160 years, Siemens Mobility is constantly innovating its portfolio in its core areas of rolling stock, rail automation and electrification, turnkey systems, intelligent traffic systems as well as related services. With digitalization, Siemens Mobility is enabling mobility operators worldwide to make infrastructure intelligent, increase value sustainably over the entire lifecycle, enhance passenger experience and guarantee availability. In fiscal year 2021, which ended on September 30, 2021, Siemens Mobility posted revenue of €9.2 billion and had around 39,500 employees worldwide. Further information is available at: www.siemens.com/mobility.
Read more

Contact

Silke Thomson-Pottebohm

Siemens Mobility GmbH

+49 174 306 3307

Chris Mckniff

Siemens Mobility GmbH

+1 646-715-6423