Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release02 November 2026Digital IndustriesErlangen
Siemens launches new ELV drive solution for AGVs and mobile robotics
Sinamics E210 and Simotics E-1EE1 form a new ELV drive solution for mobile applications
Sinamics E210: Compact ELV converter for mobile applications
The new Sinamics E210 has been specifically designed for battery-powered 24 V and 48 V applications. As a compact regenerative converter, it enables precise and safe control of traction and wheel drives as well as other motion axes, including steering, lifting, and auxiliary axes. Direct connection to ELV battery systems eliminates the need for additional voltage conversion, simplifying system architecture and improving energy efficiency. Integrated safety functions, PROFIsafe support, PROFINET IRT communication, and seamless integration into TIA Portal and Simove enable rapid implementation in modern vehicle designs. Thanks to its compact design, high overload capability, and flexible installation options, the converter is ideally suited for the next generation of high-performance AGVs and AMRs.
Simotics E-1EE1: New servomotors for high-performance ELV applications
With the new Simotics
E-1EE1 motors in shaft heights 40 to 63, Siemens is strategically expanding its
motor portfolio for extra-low-voltage applications into higher power and torque
ranges. Designed for 24 V and 48 V systems, the servomotors are optimally
matched to the Sinamics E210 and are particularly suitable for dynamic mobile
applications. An absolute 14-bit BiSS-C safety encoder and the internal
dual-channel design support safety-related applications up to SIL 2. The
electronic nameplate enables the Sinamics E210 to automatically read relevant
motor data, simplifying parameterization and commissioning. Optional holding
brakes, various gearbox options, and flexible connection technology further
allow adaptation to a wide range of vehicle and machine concepts.
An integrated Siemens solution for the mobile intralogistics systems of tomorrow
With the Sinamics E210
converter and Simotics E-1EE1 motors, Siemens provides a new, integrated drive
solution for the growing requirements of mobile intralogistics applications.
The combination of converter, motor, integrated safety, simplified engineering,
and automation enables manufacturers of AGVs, AMRs, and other mobile platforms
to accelerate development, reduce integration risks, and achieve long-term
investment security. As part of the Siemens ecosystem, users benefit not only
from high-performance drive technology but also from a scalable system
architecture capable of supporting future requirements in automation, safety,
and cybersecurity.
For this press release
Siemens Digital Industries (DI) empowers companies of all sizes within the process and discrete manufacturing industries to accelerate their digital and sustainability transformation across the entire value chain. Siemens’ cutting-edge automation and software portfolio revolutionizes the design, realization and optimization of products and production. And with Siemens Xcelerator – the open digital business platform – this process is made even easier, faster, and scalable. Together with our partners and ecosystem, Siemens Digital Industries enables customers to become a Digital Enterprise. Siemens Digital Industries has a workforce of around 70,000 people worldwide.
Siemens AG (Berlin and Munich) is a leading technology company focused on industry, infrastructure, mobility, and healthcare. The company’s purpose is to create technology to transform the everyday, for everyone. By combining the real and the digital worlds, Siemens empowers customers to accelerate their digital and sustainability transformations, making factories more efficient, cities more livable, and transportation more sustainable. A leader in industrial AI, Siemens leverages its deep domain know-how to apply AI – including generative AI – to real-world applications, making AI accessible and impactful for customers across diverse industries. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a leading global medical technology provider pioneering breakthroughs in healthcare. For everyone. Everywhere. Sustainably. In fiscal 2025, which ended on September 30, 2025, the Siemens Group generated revenue of €78.9 billion and net income of €10.4 billion. As of September 30, 2025, the company employed around 318,000 people worldwide on the basis of continuing operations. Further information is available on the Internet at www.siemens.com.