Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Siemens launches intelligent link module to boost industrial automation data transparency

SIRIUS 3RC7 Intelligent Link Modules

“Transparency down to field level is becoming increasingly important. However, many devices are not connected to the automation system, which means important data is missing. By digitalizing the field level, we are creating a new dimension of transparency and enabling data-driven decisions,” said Andreas Matthé, CEO of Electrical Products at Siemens Smart Infrastructure.
A variety of load feeder parameters can be collected and evaluated directly, including voltage, current, phase imbalance, number of overload trips, and much more. The integrated diagnostic functions help detect and correct faults more quickly. Among other things, the data can be used for Senseye Predictive Maintenance, Siemens’ comprehensive solution for predictive maintenance. It uses artificial intelligence, for example to examine current fluctuations for anomalies that indicate a defect. This significantly increases the planning reliability for maintenance, availability, and cost-effectiveness of the system.
Thanks to full integration in TIA, users receive up-to-date status information in their operating software. In addition, when using special apps such as Node-RED, they have access to a dashboard to quickly identify bottlenecks. This prevents downtime and increases the availability of the system.
The SIRIUS 3RC7 intelligent link modules integrate perfectly into the compact SIMATIC ET 200SP I/O system as well as any other common automation system. Up to 16 load feeders can be connected per BA-Send module bus adapter in order to benefit from the simple commissioning, individual scalability, and maximum flexibility offered by the SIMATIC ET 200SP.
In conjunction with SIRIUS switchgear and the compact SIMATIC ET 200SP I/O system for control cabinets, SIRIUS 3RC7 intelligent link modules ensure reliable and efficient data exchange between OT and IT. The addition of the new SIRIUS 3RC7 intelligent link module to the existing SIRIUS portfolio (modular system) has created a new, enhanced product: the SIRIUS Intelligent Load Feeder. The SIRIUS Intelligent Load Feeder is a pre-assembled digital feeder consisting of a SIRIUS 3RV2 circuit breaker, a SIRIUS 3RT2 contactor, and the intelligent link module.

SIRIUS 3RC7 Intelligent Link Modules combined with SIMATIC ET 200SP

Siemens Smart Infrastructure (SI) is shaping the market for intelligent, adaptive infrastructure for today and the future. It addresses the pressing challenges of urbanization and climate change by connecting energy systems, buildings, and industries. SI provides customers with a comprehensive end-to-end portfolio from a single source – with products, systems, solutions, and services from the point of power generation all the way to consumption. With an increasingly digitalized ecosystem, it helps customers thrive and communities progress while contributing toward protecting the planet. Siemens Smart Infrastructure has its global headquarters in Zug, Switzerland. As of September 30, 2023, the business had around 75,000 employees worldwide. 
Read more
Siemens AG (Berlin and Munich) is a leading technology company focused on industry, infrastructure, mobility, and healthcare. The company’s purpose is to create technology to transform the everyday, for everyone. By combining the real and the digital worlds, Siemens empowers customers to accelerate their digital and sustainability transformations, making factories more efficient, cities more livable, and transportation more sustainable. Siemens also owns a majority stake in the publicly listed company, Siemens Healthineers, a leading global medical technology provider shaping the future of healthcare. In fiscal 2023, which ended on September 30, 2023, the Siemens Group generated revenue of €74.9 billion and net income of €8.5 billion. As of September 30, 2023, the company employed around 305,000 people worldwide on the basis of continuing operations. Further information is available on the Internet at www.siemens.com.
Read more
Reference Number: HQSIPR202410157022EN

Contact

Christian S. Wilson 

Siemens Smart Infrastructure

+49 172 138 5608