[{"name":"Home","site_name":"Press | Company | Siemens","description":"","url_str":"\/global\/","level":0,"image":"","base_root":"https:\/\/press.siemens.com","base_nid":"5","base_nodepath":"\/node\/5","base_path":"\/global\/","base_secure_url":"https:\/\/press.siemens.com\/global","children":null}]
[]
Please use another Browser
It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and
usability.
For the best experience we suggest that you download the newest version of a supported browser:
Versatile solution for retrofit applications and new projects
Maintenance-free vacuum technology with up to 10,000 CO operating cycles
Manitoba Hydro to harness the power of new SF6-free generator circuit-breaker system
Siemens is expanding its generator circuit-breaker portfolio with a new
compact version - the HB1-Compact (HB1-C). The versatile and highly
customizable solution uses maintenance-free vacuum switching technology and
addresses the most challenging of constraints. Available in L-shape and I-shape
designs, the HB1-C can be mounted either vertically or horizontally and can be
adjusted to match existing busbar connection points. Additionally, the
generator circuit-breaker and its integrated main disconnector can be fitted
with earthing switches on the generator side and/or the transformer side for
greater flexibility.
Versatile solution for retrofit applications and new projects
Maintenance-free vacuum technology with up to 10,000 CO operating cycles
Manitoba Hydro to harness the power of new SF6-free generator circuit-breaker system
Siemens is expanding its generator circuit-breaker portfolio with a new
compact version - the HB1-Compact (HB1-C). The versatile and highly
customizable solution uses maintenance-free vacuum switching technology and
addresses the most challenging of constraints. Available in L-shape and I-shape
designs, the HB1-C can be mounted either vertically or horizontally and can be
adjusted to match existing busbar connection points. Additionally, the
generator circuit-breaker and its integrated main disconnector can be fitted
with earthing switches on the generator side and/or the transformer side for
greater flexibility.
The HB1-C generator circuit-breaker
These customizable features make the HB1-C not only suitable for new applications,
but also valuable for retrofit scenarios in power plants where security of
supply is essential, and space is often limited. The HB1-C is to be showcased at Enlit Europe, taking place in Frankfurt
from November 29 to December 1.
With increased focus on renewable power and cost reduction front of
mind, reliable protection technology is crucial. Generator circuit-breakers are
vital components for improving the reliability and availability of power
plants. Their installation not only protects equipment such as generators and
transformers against overload or short circuiting, but also provides high
availability, simplified operational procedures and a reduction in costs.
Manitoba Hydro, the electric power and natural gas utility in the
province of Manitoba, Canada is set to reap the rewards of the new HB1-Compact
model. Thanks to a contract with Siemens Canada, Manitoba Hydro will install up
to twelve replacement generator circuit-breaker systems in its 1,220 MW Kettle
Generating Station, located on the lower Nelson River in Manitoba. The contract
underpins a long-term relationship between Siemens and Manitoba Hydro, as the
two organisations work together to extend the life of this important generating
station and to continue to deliver clean, renewable, and dispatchable energy
for the province of Manitoba.
Offering the highest levels of customization, the HB1-Compact model provides
power plant operators with the greatest degree of flexibility when designing a
new plant or replacing outdated equipment. Designed with reliability also at
its core, the HB1-C’s full-spring operating mechanism has been selected by
CIGRE as the most reliable way to operate a generator circuit-breaker with a
lifespan of up to 10,000 operating cycles. With all components and functions
type and routine tested together, the HB1-C delivers a native interlocking
system with the highest levels of reliability and safety. Indeed, to guarantee
safe maintenance, the circuit-breaker can be fitted with integrated line and
earth disconnecting switches.
Circuit-breaker in I-shape design
Also available in L-shape
With cost savings a key concern for many plant operators, the HB1-C is
designed to reduce costs during the project implementation and ongoing operations.
Its simple and compact design means that transport costs are reduced and outage
times for the installation of a new circuit-breaker are minimal. Costs are
further reduced thanks to the maintenance-free vacuum switching technology which
eliminates the need for gas handling, guarantees minimum maintenance costs and
increases the recycling rate of the systems.
Siemens Smart Infrastructure (SI) is shaping the market for intelligent, adaptive infrastructure for today and the future. It addresses the pressing challenges of urbanization and climate change by connecting energy systems, buildings and industries. SI provides customers with a comprehensive end-to-end portfolio from a single source – with products, systems, solutions and services from the point of power generation all the way to consumption. With an increasingly digitalized ecosystem, it helps customers thrive and communities progress while contributing toward protecting the planet. Siemens Smart Infrastructure has its global headquarters in Zug, Switzerland. As of September 30, 2021, the business had around 70,400 employees worldwide.
Siemens AG (Berlin and Munich) is a technology company focused on industry, infrastructure, transport, and healthcare. From more resource-efficient factories, resilient supply chains, and smarter buildings and grids, to cleaner and more comfortable transportation as well as advanced healthcare, the company creates technology with purpose adding real value for customers. By combining the real and the digital worlds, Siemens empowers its customers to transform their industries and markets, helping them to transform the everyday for billions of people. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a globally leading medical technology provider shaping the future of healthcare. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the transmission and generation of electrical power.
In fiscal 2022, which ended on September 30, 2022, the Siemens Group generated revenue of €72.0 billion and net income of €4.4 billion. As of September 30, 2022, the company had around 311,000 employees worldwide. Further information is available on the Internet at
www.siemens.com.