Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release12 April 2023Smart InfrastructureZug
Siemens innovates with new sensor bushing, protection and indication devices

SIPROTEC 7SY82 Universal Protection Device with LPIT inputs in combination with SIBushings
Designed for compact,
intelligent secondary substations, the SICAM FCM plus provides
system operators with a solution for fast fault location and more transparency
in the distribution grid. It is suitable for grounded,
isolated, and compensated networks. Moreover, SICAM FCM plus offers reduced
cost of installation and minimal maintenance, while its adaptive integrated
temperature compensation algorithm enables high-precision measurement without
calibration and adjustment to the primary operating voltages and currents.
“An
integrated approach to medium voltage power distribution is essential for
energy-efficient infrastructure, buildings, and industrial applications.
Through continued investment in all areas of our Electrification and Automation
solutions, we are able to work with customers to ensure
a reliable and resilient supply that also aids them in achieving their sustainability
goals,” says Stephan May, CEO Electrification and Automation at Siemens Smart
Infrastructure. “We look forward to showcasing our expanded portfolio at the
upcoming Hannover Messe.”
Also being
unveiled at the event is the SIPROTEC 7SY82, a multifunctional protection
device with LPIT inputs. This universal protection device joins the renowned
SIPROTEC 5 product family of field devices for protection, control, monitoring,
and measuring applications in electrical energy systems.
LPITs in
combination with the universal SIPROTEC 7SY82 minimize device variance. As a
result, customers optimize their investment and operating costs, gain time in
project planning, and achieve significant savings in terms of logistics and spare parts. Additionally, LPIT
technology enables customers to increase the sustainability and reduce the
ecological footprint of their medium voltage switchgear. Due to the new
measuring inputs which conform with the instrument transformer standard IEC
61869, it is possible to connect sensors that consume less power, are safer for
operating personnel and use less materials
such as iron, copper and cast resin, compared to conventional instrument
transformers.
The SIBushing with SICAM FCM plus and SIPROTEC
7SY82 are to be showcased at the upcoming Hannover
Messe, taking place from April 17th to 21st. Free Tickets are available to join the event.
For further information on Siemens Smart
Infrastructure, please see
www.siemens.com/smart-infrastructure
www.siemens.com/smart-infrastructure
For this press release
Follow us on Twitter
Siemens Smart Infrastructure (SI) is shaping the market for intelligent, adaptive infrastructure for today and the future. It addresses the pressing challenges of urbanization and climate change by connecting energy systems, buildings and industries. SI provides customers with a comprehensive end-to-end portfolio from a single source – with products, systems, solutions and services from the point of power generation all the way to consumption. With an increasingly digitalized ecosystem, it helps customers thrive and communities progress while contributing toward protecting the planet. Siemens Smart Infrastructure has its global headquarters in Zug, Switzerland. As of September 30, 2022, the business had around 72,700 employees worldwide
Siemens AG (Berlin and Munich) is a technology company focused on industry, infrastructure, transport, and healthcare. From more resource-efficient factories, resilient supply chains, and smarter buildings and grids, to cleaner and more comfortable transportation as well as advanced healthcare, the company creates technology with purpose adding real value for customers. By combining the real and the digital worlds, Siemens empowers its customers to transform their industries and markets, helping them to transform the everyday for billions of people. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a globally leading medical technology provider shaping the future of healthcare. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the transmission and generation of electrical power.
In fiscal 2022, which ended on September 30, 2022, the Siemens Group generated revenue of €72.0 billion and net income of €4.4 billion. As of September 30, 2022, the company had around 311,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
In fiscal 2022, which ended on September 30, 2022, the Siemens Group generated revenue of €72.0 billion and net income of €4.4 billion. As of September 30, 2022, the company had around 311,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Reference Number: HQSIPR202304116678EN