Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release18 July 2017Building TechnologiesZug
Siemens expands damper actuator family

The picture shows the damper actuator from Siemens
With the new 4 Nm-torque spring-return actuators, Building Technologies can more finely scale air damper motorization, thus avoiding unnecessary and expensive over-motorization. Spring-return actuators are primarily used when spring force is needed to move de-energized air dampers (e.g., power failure) into a defined fail-safe position.
The new conventional damper actuators with 2 Nm torque are now available for AC 230 V as well as AC/DC 24 V. This means greater flexibility and less effort during installation because no additional power supply needs to be installed, regardless of the controller's specifications. Other variants with DC 0/2-10 V control signals for continuously modulating actuators and for non-modulating actuators with 2/3- positions open up new control options for damper actuators.
The 2 Nm damper actuators are suitable not only for ventilation applications but also water applications, such as heated and chilled ceilings. There they contribute to a cost-efficient solution using the new DN10 6-way control ball valves from Siemens.
All the new damper actuators are equipped with a left-right switch that allows the direction of rotation to be changed without added cabling effort. With an IP54 protection class, the new models are highly resistant to dust and water and hence offer greater reliability during operation.
The modern air damper actuators of the OpenAir family are fast and easy to install thanks to the new one-screw shaft adapter. Other quality hallmarks include extreme robustness and long product life of approximately 100,000 full and 5,000,000 partial cycles.
Like all products in the OpenAir family, the new damper actuators have a printed data matrix code that allows instant online access to product information (datasheets, installation instructions etc.).
For more information about the Building Technologies Division, please visit www.siemens.com/buildingtechnologies.
For more information about OpenAir damper actuators, please visit www.siemens.com/openair.
For further information on #CreatingPerfectPlaces, please see
Landing Page: www.siemens.com/perfect-places
Landing Page: www.siemens.com/perfect-places
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Reference Number: PR2017070358BTEN