Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release04 October 2017Energy ManagementErlangen
Siemens' EnergyIP smart grid applications run on the IoT operating system MindSphere

EUW 2017
Numerous EnergyIP applications have been successfully used around the world for years. They include applications for meter data management and distributed energy management, energy efficiency applications for the energy sector and for industry, and various applications for data analysis, such as load prediction in the grid and tracing system losses. There are also EnergyIP applications for power outage management and for managing the equipment and systems in substations.
"Energy management applications that run reliably on EnergyIP will run just as reliably on MindSphere. This will create additional added value for our customers by enabling them to more easily combine grid status data with data in other applications fields, such as power generation, in industry and everywhere else that MindSphere is being used in the future," said Thomas Zimmermann, CEO of the Digital Grid Business Unit in the Energy Management Division of Siemens. "The evolution of our energy systems is in full swing, and data is the new fuel for energy suppliers. Innovative IoT technologies are essential if our customers are to use the data to derive value for their businesses. We are developing the right applications for this, relying on standard protocols. This enables us to keep the platform flexible and at the same time open for developers from third parties across our own applications."
The Internet of Things (IoT) will also play an increasing role for energy suppliers and network operators because as digitalization progresses, it will be necessary to install additional equipment like protection and automation devices in the grids. These devices must be efficiently installed, operated, and renewed. To operate them efficiently and at optimal performance over their lifecycle, and to create more value for the energy supplier using data analysis, sophisticated IoT technologies – like the EnergyIP applications under MindSphere – will be required. EnergyIP applications will continue to evolve for data acquisition and analysis and for managing and evaluating all energy-relevant data. The goal is to help energy suppliers and grid operators cope more readily with the digitalization process that is taking place throughout the energy industry.
At Siemens, the Energy Management Division brings together its extensive IoT-portfolio of software and digital services under "MindSphere for Energy." The portfolio combines the topics of MindSphere and energy. It is designed to enable power utilities and grid operators to benefit from the impact of the Internet of Things on the energy sector. Siemens thus offers an IoT portfolio with a unique depth, breadth, and openness. This special depth of offerings is based on the outstanding domain knowledge of Siemens in terms of the ability to connect all devices, systems, and installations in power grids to MindSphere. Yet it also represents a wide range of industry-specific applications from the established EnergyIP series, with 75 million licenses for smart meters sold worldwide. The special range of offerings include end-to-end solutions for sector coupling and cross-industry application fields such as intelligent e-mobility network solutions or the integration into factory automation. Last but not least, an open platform and an open partner ecosystem are available so that, for example, third parties can also develop MindSphere applications.
For more information on EnergyIP, please see
www.Siemens.com/energyip
For more information on EnergyIP, please see
www.Siemens.com/energyip
Further information on MindSphere is available at www.siemens.com/global/en/home/products/software/mindsphere.html
More press material on EUW 2017 is available at
www.siemens.com/press/euw2017
www.siemens.com/press/euw2017
For more information on Division Energy Management:
www.siemens.com/energy-management
www.siemens.com/energy-management
For this press release
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Dietrich Biester
Siemens AG
Freyeslebenstr. 1
91058 Erlangen
Germany
91058 Erlangen
Germany
+49 (9131) 7-33559