Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release27 February 2018MobilityMunich
Siemens delivers signaling for a fully automated metro in Malaysia
The new line, with 38 kilometers and one depot, is expected to be completed in February 2021. The scope for Siemens also includes the installation of an intrusion preventive system (IPS) and a platform screen door system (PSD).
"With public transportation being a decisive factor for the economic growth of the Greater Kuala Lumpur area, this project will support the development of an attractive, reliable and efficient mass transit infrastructure by optimizing headway times and improving punctuality through our cutting-edge Communication Based Train Control (CBTC) technology Trainguard MT, which enables the operator to maximize their network capacity and throughput," said Michael Peter, CEO of Siemens Mobility Division.
The planned route for the LRT3 will ultimately link Bandar Utama to Klang, spanning 26 stations – 25 elevated above ground and one underground. Once completed, the line will be incorporated into the existing Klang Valley Integrated Transit System in the city. It will provide connectivity to the western part of the Greater Kuala Lumpur/Klang Valley area. The project is expected to benefit 74,000 commuters daily and 500,000 residents as it will mobilize 36,720 passengers per hour in a single direction by improving connectivity and reducing traffic congestion.
The LRT3 line will be fully automated with Grade of Automation 4 (GoA4). As of 2016, Siemens has equipped about 300 kilometers of lines worldwide with signaling technology for fully automated operations.
For further information about the Mobility Division, please see: www.siemens.com/mobility
For this press release
@SiemensMobility
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 377,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Anne-Muriel Alexici
Siemens AG
Otto-Hahn-Ring 6
81739 Munich
Germany
81739 Munich
Germany
+49 (89) 636-24407