Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release25 September 2019Gas and PowerHouston
Siemens to build industrial power plant at the Marl Chemical Park in Germany
“In building this power plant, whose technical and commercial concept was worked out jointly between Siemens and Evonik, we’re helping Evonik significantly cut its CO2 emissions,” said Michael Becker, CFO of Siemens Gas and Power. “In addition, the state-of-the-art plant will ensure a reliable supply of electricity and process steam for the chemical park. The ability to use various gases as fuel is another benefit and further increases the plant’s economic feasibility.”
“In deciding to build the new power plant, we’re ending our coal-based production of electricity and steam in Marl after more than 80 years, and cutting the direct annual greenhouse gas emissions of our plants by nearly one fifth worldwide,” said Thomas Wessel, Chief Human Resources Officer at Evonik. “We are pleased to have Siemens at our side, a reliable partner who is helping us to achieve our ambitious climate goals.”
“Siemens Financial Services’ structuring expertise and experience in the energy sector for years enabled us to offer a financing solution tailored to the customer’s needs,” said Veronika Bienert, CFO of Siemens Financial Services GmbH. “This made it possible to implement the project in close cooperation with Siemens Gas and Power, which is providing the technology and service activities.”
Siemens’ scope of supply includes the turnkey construction of two identical power plant units as well as one industrial gas turbine, and one industrial steam turbine for each unit. It also includes generators, auxiliary systems, and the control system.
Siemens will carry out preventive maintenance work on both gas turbines for a period of 15 years under a long-term service agreement. This agreement also covers remote diagnostic services for daily plant monitoring and monthly analyses of the operating data. These digital services will ensure high plant availability.
Thanks to the use of special heat recovery steam generators and catalysts, the system can operate on natural gas as well as re-gasified liquefied natural gas (LNG), and various other gases, such as residual gas from production processes. Each power plant unit can produce not only electricity but also up to 220 metric tons of process steam per hour. Thanks to the plant’s high flexibility that enables it to compensate for the fluctuating infeed of renewable energy into the power grid and its ability to produce district heat, it is also supporting the energy transition in Germany.
For further information on Siemens Gas and Power, please see www.siemens.com/energy
For further information on industrial energy solutions from siemens, please see www.siemens.com/industrial-energy
For further information on industrial energy solutions from siemens, please see www.siemens.com/industrial-energy

The new combined cycle power plant, which is being built in
the Marl chemical park in North Rhine-Westphalia, will consist of two units,
each with an electrical capacity of 90 megawatts. Each unit will be able to
produce electricity as well as process steam and district heat. The plant’s
fuel efficiency will thus exceed 90 percent.
For this press release
Siemens Gas and Power (GP) is a global pacesetter in energy, helping customers to meet the evolving demands of today’s industries and societies. GP comprises broad competencies across the entire energy value chain and offers a uniquely comprehensive portfolio for utilities, independent power producers, transmission system operators, the oil and gas industry and other energy intensive industries. Products, solutions, systems and services address the extraction, processing and the transport of oil and gas as well as power and heat generation in central and distributed thermal power plants, power transmission and grid stability, as well as energy transition technologies including storage. With global headquarters in Houston in the U.S. and more than 64,000 employees in over 80 countries, Siemens Gas and Power has a presence across the globe and is a leading innovator for the energy systems of today and tomorrow, as it has been for more than 150 years.
Siemens AG (Berlin and Munich) is a
global technology powerhouse that has stood for engineering excellence,
innovation, quality, reliability and internationality for more than
170 years. The company is active around the globe, focusing on the areas
of power generation and distribution, intelligent infrastructure for buildings
and distributed energy systems, and automation and digitalization in the
process and manufacturing industries. Through the separately managed company
Siemens Mobility, a leading supplier of smart mobility solutions for rail and
road transport, Siemens is shaping the world market for passenger and freight
services. Due to its majority stakes in the publicly listed companies Siemens
Healthineers AG and Siemens Gamesa Renewable Energy, Siemens is also a
world-leading supplier of medical technology and digital healthcare services as
well as environmentally friendly solutions for onshore and offshore wind power
generation. In fiscal 2018, which ended on September 30, 2018, Siemens
generated revenue of €83.0 billion and net income of €6.1 billion. At
the end of September 2018, the company had around 379,000 employees worldwide.
Further information is available on the Internet at www.siemens.com
.
Contact
Christina Hümmer
Gas and Power
Freyeslebenstr. 1
91058 Erlangen
Germany
91058 Erlangen
Germany
+49 (9131) 17-45722