Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release02 October 2018Power and GasHouston
Siemens and Southern Idaho Solid Waste announce commissioning of landfill gas-to-energy project
Decomposing waste gives off massive amounts of greenhouse gases, especially methane. SISW engineers worked with Siemens and Siemens' channel partner, Industrial-Irrigation Services, to develop a solution that would capture the methane for use as a fuel gas to produce electricity. "We saw this gas and realized we were just wasting it by burning it for no productive use," said SISW's environmental manager, Nate Francisco.
To capture methane and convert it into electricity, the Milner Butte Landfill deployed two Siemens SGE-56HM gas generator sets to run on the waste gas from the landfill and generate electrical power. Once the landfill gas is converted to electricity, it is transported to Idaho Power through a 20-year purchase agreement and is used by the community as a low-cost source of power. To date, the two engines have been generating enough power for approximately 2,000 homes. Each set is rated at
1,300kWe and includes generator controls and a power panel.
1,300kWe and includes generator controls and a power panel.
Siemens SGE-HM series is purpose-built for landfill gas-to-energy power applications. By incorporating advanced technology and design into the cylinder heads, valves, camshafts, and turbochargers, the SGE-56HM engine provides customers like SISW with a high-performing low-operating-cost solution.
"We expect these engines to remain in operation for 20 to 30 years," said Josh Bartlome, executive director at SISW. "They're big engines built for endurance."
SISW estimates that within the next 20 years the facility will generate approximately $36 million in revenue, netting about a third of that after costs and inflation. Creating a long-term revenue generator like this model used by SISW will allow the District to realize lower power costs.
"The Milner Butte Landfill project represents the future of distributed power," said Chris Nagle, North American Regional Director for Siemens Gas Engines business. "This plant assists the local community with its power needs while being environmentally responsible. Siemens is proud to support SISW and Industrial-Irrigation Services with this project."
For further information on Siemens Gas Engines, please see: https://sie.ag/2MOzVRJ
For this press release
@Siemens_Energy
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 377,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Janet Ofano
Siemens AG
5101 Westinghouse Boulevard
28273-9640 Charlotte, NC
USA
28273-9640 Charlotte, NC
USA
+1 803-389-6753