Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Performance enhancements for Advanced Controllers for automation

The picture shows the Advanced Controllers for automation.

The two fail-safe 1511TF-1 PN and 1515TF-2 PN technology CPUs are new additions to the portfolio of the Simatic S7-1500 Advanced Controller. The fail-safe Simatic S7-1500 T-CPUs from Siemens combine extended motion control functionalities, such as gearing and camming, with safety-related applications in a single device. Together with the already existing, fail-safe 1517TF-3 PN/DP T-CPU, which is used for more complex applications, they complete the portfolio of technology CPUs. The Simatic S7-1500 Advanced Controller has a functionally and fully scalable portfolio available to the user for standard, safety and motion control tasks.
The Simatic S7-1500 T-CPUs are specifically matched with Sinamics V90 PN and Sinamics S210 servo drive systems for mid-range motion control applications: The new Sinamics S210 servo drive system is available in five performance classes ranging from 50 to 750 watts. The many possible motion control applications focus on dynamic movement and processing – such as positioning, conveying and winding. The fully scalable motion control solutions can be implemented efficiently in the Engineering Framework TIA Portal with technology objects, integrated diagnostics and detailed error detection.
The new PS 60W 24/48/60 V DC HF power supply module for the Simatic S7-1500 Advanced Controller buffers the energy in the event of power failures. Without a battery and therefore maintenance-free, the new power supply module offers full data remanence of up to 20 megabytes for the CPUs. It feeds directly into the backplane bus and supports the integrated diagnostic modules of the S7-1500 system – for standard, safety and motion control applications. This speeds up the restart of machines and plants, as the data is still there when the power returns, and the parameters do not need to be reset. The new power supply module now also allows production applications for which the Simatic S7-400 was previously used to be converted to up-to-date Simatic S7-1500 technology with no limitation of the remanence behavior.

For additional information, see www.siemens.com/s7-1500
For further information on Siemens at the Hannover Messe 2017, please see www.siemens.com/press/hm17 and www.siemens.com/hannovermesse
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Read more
Reference Number: PR2017040246DFEN

Contact

Gerhard Stauss

Siemens AG

Gleiwitzer Str. 555
90475 Nuremberg
Germany

+49 (911) 895-7945