[{"name":"Home","site_name":"Press | Company | Siemens","description":"","url_str":"\/global\/","level":0,"image":"","base_root":"https:\/\/press.siemens.com","base_nid":"5","base_nodepath":"\/node\/5","base_path":"\/global\/","base_secure_url":"https:\/\/press.siemens.com\/global","children":null}]
[]
Please use another Browser
It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and
usability.
For the best experience we suggest that you download the newest version of a supported browser:
Press Release04 January 2022Smart InfrastructureZug
New KNX binary inputs expand DIN-rail
mounted device portfolio from Siemens
Extensive operating and control functions as a convenient interface to KNX systems
Suitable for sophisticated multi-discipline applications such as colored light control and access control
Clear, intuitive direct operation via membrane keypad and with LED status display
Siemens Smart Infrastructure has added two
new variants of KNX binary inputs to its portfolio of DIN-rail mounted devices:
The new binary inputs N 262 and N 263 offer easy installation and intuitive
operation and are available as potential-free and voltage-loaded versions in
widths of 4 MU (4 binary inputs) and 8 MU (8 binary inputs).
Extensive operating and control functions as a convenient interface to KNX systems
Suitable for sophisticated multi-discipline applications such as colored light control and access control
Clear, intuitive direct operation via membrane keypad and with LED status display
Siemens Smart Infrastructure has added two
new variants of KNX binary inputs to its portfolio of DIN-rail mounted devices:
The new binary inputs N 262 and N 263 offer easy installation and intuitive
operation and are available as potential-free and voltage-loaded versions in
widths of 4 MU (4 binary inputs) and 8 MU (8 binary inputs).
The new binary inputs can be used to detect
switching and system states or to count pulses with threshold monitoring. In
addition to switching and dimming lights or controlling blinds, the devices
also support sophisticated tasks for multi-discipline applications such as
colored light control, logic operations, or differential pulse counting. This
makes it possible, for example, to implement an access control solution that
detects the current number of persons in a room.
In addition, the potential-free binary
inputs can be used to evaluate window, door and other signal contacts.
Depending on whether a window is open or closed, the room operating mode can be
set to frost or heat protection during heating or cooling.
Unlike their predecessor models, the new binary inputs N 262 and N 263 have all
the characteristic benefits of the current generation of DIN-rail mounted
devices from Siemens. This includes uniform housing concept, device labeling,
maintenance-free terminals, supply of the device electronics via the KNX bus
and bus terminals. In addition, the devices have a uniformly placed
programming/LED and, for the first time, a direct operating level with status
display. They are part of a consistent software concept and support multi-mode
(KNX S-Mode and PL-Link).
Easy
installation and intuitive direct operation
The maintenance-free terminals ensure quick
and easy installation as well as maximum flexibility. The clear and intuitive
direct operating level allows the simulation of input states during
commissioning: Conventional switches, push-buttons or potential-free or
voltage-loaded contacts do not need to be connected. Wide-range inputs (N 263)
for voltage signals from 10 to 230 V with separate earth connection per
channel make it possible to switch different voltage potentials.
Siemens Smart Infrastructure (SI) is shaping the market for intelligent, adaptive infrastructure for today and the future. It addresses the pressing challenges of urbanization and climate change by connecting energy systems, buildings and industries. SI provides customers with a comprehensive end-to-end portfolio from a single source – with products, systems, solutions and services from the point of power generation all the way to consumption. With an increasingly digitalized ecosystem, it helps customers thrive and communities progress while contributing toward protecting the planet. Siemens Smart Infrastructure has its global headquarters in Zug, Switzerland. As of September 30, 2021, the business had around 70,400 employees worldwide.
Siemens AG (Berlin and Munich) is a technology company focused on industry, infrastructure, transport, and healthcare. From more resource-efficient factories, resilient supply chains, and smarter buildings and grids, to cleaner and more comfortable transportation as well as advanced healthcare, the company creates technology with purpose adding real value for customers. By combining the real and the digital worlds, Siemens empowers its customers to transform their industries and markets, helping them to transform the everyday for billions of people. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a globally leading medical technology provider shaping the future of healthcare. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the transmission and generation of electrical power.
In fiscal 2021, which ended on September 30, 2021, the Siemens Group generated revenue of €62.3 billion and net income of €6.7 billion. As of September 30, 2021, the company had around 303,000 employees worldwide. Further information is available on the Internet at
www.siemens.com.