Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release21 February 2018Building TechnologiesZug
New fine dust sensor to monitor indoor climate

The picture shows the Symaro fine dust sensor from Siemens.
The new fine dust sensor is based on laser technology and measures the particle pollution of the air in two categories: PM 2.5 and PM 10, i.e. particulate matter with a diameter of 0.3 to 2.5 micrometers or 0.3 to 10 micrometers respectively. The new fine dust sensor is targeted for use in office and high-end residential buildings.
During operation, dust particles accumulate on fine dust sensors, reducing their performance over time. The Siemens sensor has a display that is activated only when the presence of people is detected. When no presence is detected in the room, the frequency of particulate matter measurements decreases, significantly improving the service life of the fine dust sensor. When the sensor module needs to be replaced, the device alerts users either on the display itself or, on models without a display, through an LED light. It is not necessary to buy a new device or reconfigure it. Replacing the sensor module is quick and easy and does not require any special skills.
The fine dust sensor has been calibrated to measure PM 2.5 particles and can be set to different air quality index (AIQ) levels to meet specific national regulations. Laser light scattering is used to measure the particulate concentration. The user interface of the device can be displayed in German, English, French and Chinese.
The fine dust sensor is the latest addition to Siemens' offering for a healthy indoor climate. Carbon dioxide (CO2) sensors help reduce the CO2 concentration of the ambient air and, conversely, increase the oxygen (O2) concentration in order to improve employee productivity. Effective temperature and humidity control decreases the risk of illnesses such as respiratory tract infections and influenza. Volatile organic compound (VOC) sensors are used to measure the harmful outgassing originating from building materials and items such as carpets and furniture. All sensors have analog signal and Modbus outputs, allowing them to be connected to Siemens heating, ventilation and air conditioning controls such as Climatix and Desigo Room Automation as well as integrated into building management systems such as Desigo CC. To achieve the desired indoor climate, the system can activate additional filters or increase the ventilation power.
The fine dust sensor is the latest addition to Siemens' offering for a healthy indoor climate. Carbon dioxide (CO2) sensors help reduce the CO2 concentration of the ambient air and, conversely, increase the oxygen (O2) concentration in order to improve employee productivity. Effective temperature and humidity control decreases the risk of illnesses such as respiratory tract infections and influenza. Volatile organic compound (VOC) sensors are used to measure the harmful outgassing originating from building materials and items such as carpets and furniture. All sensors have analog signal and Modbus outputs, allowing them to be connected to Siemens heating, ventilation and air conditioning controls such as Climatix and Desigo Room Automation as well as integrated into building management systems such as Desigo CC. To achieve the desired indoor climate, the system can activate additional filters or increase the ventilation power.
Particulate matter is inhaled through the respiratory tract and can cause lung cancer and cardiovascular diseases. People spend about 90% of their lives in buildings. For this reason, minimizing particle pollution in the ambient air is a crucial factor in protecting the health of employees. Particle pollution is a global issue; countries such as China, India and the Middle East as well as urban centers worldwide are especially at risk.
For further information on Division Building Technologies, please see www.siemens.com/buildingtechnologies
For further information on the fine dust sensor, please see www.siemens.com/symaro
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 377,000 employees worldwide. Further information is available on the Internet at www.siemens.com.