[{"name":"Home","site_name":"Press | Company | Siemens","description":"","url_str":"\/global\/","level":0,"image":"","base_root":"https:\/\/press.siemens.com","base_nid":"5","base_nodepath":"\/node\/5","base_path":"\/global\/","base_secure_url":"https:\/\/press.siemens.com\/global","children":null}]
[]
Please use another Browser
It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and
usability.
For the best experience we suggest that you download the newest version of a supported browser:
New Desigo CC V6 building management platform adds native cloud connectivity
Updated Desigo CC V6 connects to Building X, Siemens' cloud-based open platform and AI-enabled suite of applications
Enhanced cybersecurity with extended support to IEC 62443-3-3 SL2
New Flex Client features improve user experience
Fulfils BACnet B-XAWS profile for cross-domain advanced workstation and BACnet Secure Connect
Siemens Smart Infrastructure has unveiled the
latest version of Desigo CC, its integrated building management platform for
the digitalization of buildings of any size. With the software update, Desigo
CC V6 offers native cloud connectivity, an improved user experience and is among
the first building management platforms worldwide to fulfill the BACnet B-XAWS
profile for cross-domain advanced workstation and BACnet Secure Connect.
Updated Desigo CC V6 connects to Building X, Siemens' cloud-based open platform and AI-enabled suite of applications
Enhanced cybersecurity with extended support to IEC 62443-3-3 SL2
New Flex Client features improve user experience
Fulfils BACnet B-XAWS profile for cross-domain advanced workstation and BACnet Secure Connect
Siemens Smart Infrastructure has unveiled the
latest version of Desigo CC, its integrated building management platform for
the digitalization of buildings of any size. With the software update, Desigo
CC V6 offers native cloud connectivity, an improved user experience and is among
the first building management platforms worldwide to fulfill the BACnet B-XAWS
profile for cross-domain advanced workstation and BACnet Secure Connect.
Native cloud connectivity to Building X
Desigo CC now connects to the recently
launched Building X, Siemens’ cloud-based open platform and AI-enabled suite of
applications. Building operators can now monitor and manage multiple Desigo CC
sites with the Building X Operations Manager cloud application. With 24/7
access to cloud-connected buildings from anywhere, unnecessary physical site
visits are reduced and response times are improved. Using the Operations
Manager, operators now have the ability to securely connect to Flex Client, the
HTML5 client application, without a complex VPN setup. This functionality can
be enabled in countries in which Building X is currently available.
Enhanced cybersecurity
Developed, operated and maintained with cybersecurity in mind, Desigo CC meets the highest protection requirements, adding support for additional IEC 62443-3-3 SL2 scenarios. It also allows for adaptation to customers’ advanced IT infrastructure, offering improved user management and increased password security.
Advanced user experience
Along with a state-of-the-art user
interface, the Desigo CC Flex Client receives additional software features to
enhance the user experience with a focus on building automation operators. Highlights
include Log Viewer for easy and efficient log data analysis; Flex Client Report
Viewer to generate, view and download reports, and the ability to manage
recipients and groups with the new application for notifications.
These enhancements make end-users' daily
operations more intuitive and efficient, and enables seamless site operation whether
on-premise or in hybrid deployments.
Cross-domain certification
For the integration of different subsystems,
Desigo CC supports the manufacturer-independent BACnet standard, to monitor and
control all subsystems with one common BMS. Desigo CC is among the first
building management platforms certified with a cross-domain profile B‑XAWS 1.16. Desigo CC supports the profiles B‑AWS, B‑ALWS, B‑ACCWS, and profile B‑XAWS, as well as
the BACnet/SC protocol. It enables the encryption of data traffic based on
certificates, ensuring a secure connection between all BACnet devices.
With a modular design, Desigo CC has the
flexibility across different disciplines to adapt to buildings and projects of
any size. Engineer-friendly functions, workflows and migration tools also allow
for the optimization of engineering costs, and simplification of migration
projects.
Desigo CC V6 will be shown for the first
time at Light + Building 2022, in Frankfurt, Germany, October 2-6. Visit us in
Hall 11.0, B56, and read more about the Siemens presence at the show,
here.
Siemens Smart Infrastructure (SI) is shaping the market for intelligent, adaptive infrastructure for today and the future. It addresses the pressing challenges of urbanization and climate change by connecting energy systems, buildings and industries. SI provides customers with a comprehensive end-to-end portfolio from a single source – with products, systems, solutions and services from the point of power generation all the way to consumption. With an increasingly digitalized ecosystem, it helps customers thrive and communities progress while contributing toward protecting the planet. Siemens Smart Infrastructure has its global headquarters in Zug, Switzerland. As of September 30, 2021, the business had around 70,400 employees worldwide.
Siemens AG (Berlin and Munich) is a technology company focused on industry, infrastructure, transport, and healthcare. From more resource-efficient factories, resilient supply chains, and smarter buildings and grids, to cleaner and more comfortable transportation as well as advanced healthcare, the company creates technology with purpose adding real value for customers. By combining the real and the digital worlds, Siemens empowers its customers to transform their industries and markets, helping them to transform the everyday for billions of people. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a globally leading medical technology provider shaping the future of healthcare. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the transmission and generation of electrical power.
In fiscal 2021, which ended on September 30, 2021, the Siemens Group generated revenue of €62.3 billion and net income of €6.7 billion. As of September 30, 2021, the company had around 303,000 employees worldwide. Further information is available on the Internet at
www.siemens.com.