Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release15 March 2018Energy ManagementErlangen
New charging unit for cost-optimized charging of electric vehicles

The picture shows the multichannel current measuring system SEM3.
This allows them to take advantage of economical electricity rates outside of peak periods and to significantly lower electricity costs. Owners of electric vehicles can also make targeted use of own generated energy, e.g. from solar panels, thus optimizing their power consumption. VersiCharge is suitable for use in a private and semi-private environment, such as in garages, carports, and on hotel and company parking lots. It is simply mounted on the wall and is dimensioned for a power supply of 230 volts (V).
The VersiCharge is available in a single-phase version for rated currents of 20 amps (A) and 32 A, as well as in a three-phase version for a rated current of 32 A. The single-phase 32 A charging unit already contains integrated DC residual current detection for 6 mA. Depending upon the version, the charging power varies between 4.6 kilowatts (kW), 7.2 kW and 22 kW. For an average passenger car, the charging time for power of 22 kW is roughly 4 hours. The charging status is indicated by means of an LED. Via an external RFID reader, the charging process can be initiated, canceled or paused at any time.
For further information on Division Energy Management, please see www.siemens.com/energy-management
For further information on electro mobility, please see www.siemens.com/electromobility
More information about the Light+Building can be found at: www.siemens.com/press/lightbuilding-2018
For this press release
Press Event
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 377,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Heidi Fleissner
Siemens AG
Siemensstr. 10
93055 Regensburg
Germany
93055 Regensburg
Germany
+49 (941) 790-2212