Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Intelligent valve from Siemens combines energy efficiency and comfort uniquely

Intelligent valve

“The unique Adaptive Flow Optimizer makes the Intelligent Valve more efficient and competitive than conventional pressure-independent control valves (PICV). Thanks to the automatic preset function, the valve now has the ability to automatically adjust the volumetric flow presetting during operation and to control itself. This leads up to 37% of energy savings for cooling and ventilation”, said Lu Han, Head of Business Segment Connected Devices at Siemens Smart Infrastructure”.
The built-in learning mechanism is based on system demand and avoids maximum volumetric flow when it is not required. This reduces the probability that the delta T limitation control has to intervene, which would lead to a loss of comfort. Thanks to automatic presetting, installation is quick and easy because the system does not need to have power and the installer does not have to adjust each valve multiple times. As a result, the valve supports out-of-the-box installation. 
The Intelligent Valve’s self-adjustment feature makes it easy to accommodate changes of usage and, among other things, helps to continuously optimize the system and immediately detect faults and anomalies. The self-test report makes it easier to document the settings data and prove the efficiency of the system at any time. Since the report is system-generated, entry and copy errors are prevented.
In addition, the RS458 interface for connection to Modbus RTU networks facilitates integration in building automation systems and improves monitoring of operating equipment anywhere in the world. 
For more information on Siemens Smart Infrastructure, see 
www.siemens.com/smart-infrastructure
For further information on the Intelligent valve, please see 
www.siemens.com/intelligentvalve

Intelligent valve

For this press release

Press Folders

Follow us on Twitter

Siemens Smart Infrastructure (SI) is shaping the market for intelligent, adaptive infrastructure for today and the future. It addresses the pressing challenges of urbanization and climate change by connecting energy systems, buildings and industries. SI provides customers with a comprehensive end-to-end portfolio from a single source – with products, systems, solutions and services from the point of power generation all the way to consumption. With an increasingly digitalized ecosystem, it helps customers thrive and communities progress while contributing toward protecting the planet. SI creates environments that care. Siemens Smart Infrastructure has its global headquarters in Zug, Switzerland. As of September 30, 2020, the business had around 69,600 employees worldwide.
Read more
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. Active around the world, the company focuses on intelligent infrastructure for buildings and distributed energy systems and on automation and digitalization in the process and manufacturing industries. Siemens brings together the digital and physical worlds to benefit customers and society. Through Mobility, a leading supplier of intelligent mobility solutions for rail and road transport, Siemens is helping to shape the world market for passenger and freight services. Via its majority stake in the publicly listed company Siemens Healthineers, Siemens is also a world-leading supplier of medical technology and digital health services. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the transmission and generation of electrical power that has been listed on the stock exchange since September 28, 2020. In fiscal 2020, which ended on September 30, 2020, the Siemens Group generated revenue of €57.1 billion and net income of €4.2 billion. As of September 30, 2020, the company had around 293,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Read more
Reference Number: HQSIPR202109296311EN

Contact

Katharina Sipura  

Siemens AG

+41 796507005