Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release05 June 2018Process Industries and DrivesNuremberg
Industrial router for secured remote access to plants and machines with Profibus

The picture shows the industrial routers Scalance M804PB
Siemens is extending its portfolio of industrial routers with the Scalance M804PB. This device allows existing machines and plants (for example with Simatic S7-300/S7-400) to be connected to Ethernet networks via Profibus/MPI (Multi-Point Interface).
The device has integrated TIA Portal cloud connector functionality. This allows users to easily access existing Profibus units from centrally administered engineering tools such as the TIA Portal or Step 7 (from version 5.5). The Scalance M804PB is a Profibus/MPI router for private, wired networks even with existing two-wire cabling. In addition to a Profibus/MPI connection, it also has two RJ45 interfaces in the form of a fast Ethernet two-port switch. It also has a C-Plug/Key-Plug slot. The Scalance M804PB supports VLAN, Firewall/VPN (IPsec)/NAT, OpenVPN (as client), VRRP/RSTP and can be configured for CLI and SNMP via web-based management tools. Download and upload data rates of 9.6 Kbit/s to 12 Mbit/s can be achieved on the Profibus/MPI interface. The redundant supply voltage is DC 24 V. Mounting options include wall mounting, DIN rails and S7-300 or S7-1500 profile rails. The Scalance M804PB Profibus/MPI router has the same user interface and comparable performance characteristics as the Scalance M-800 and S615 product line as it is based on the same firmware. This provides easy handling and compatibility with existing systems (for example, the Simatic portfolio, network management software etc.). For example, with the Scalance M804PB, digital input and output allow on-site access control via key switches.
For further information, refer to www.siemens.com/scalance-m
Find further information about Siemens at the Achema 2018 at www.siemens.com/achema and www.siemens.com/press/achema2018
For this press release

Event: Achema 2018
Press Event
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 377,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
David Petry
Siemens AG
Werner-von-Siemens-Str. 65
91052 Erlangen
Germany
91052 Erlangen
Germany
+49 (9131) 7-26616