Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release11 June 2018Process Industries and DrivesNuremberg
High safety level under extreme conditions: Simotics XP Chemstar
Simotics XP - a platform concept for explosion-proof low-voltage motors.
Based on many decades of experience and expertise in explosion protection, Siemens has united its classic Chemstar product range with the properties of its proven Simotics XP low-voltage motor platform. The new generation of motors are available in a range from 0.25 to 500 kilowatts (kW) covering the ignition protection spectrum for zones 1, 2, 21 and 22 in Ex db, Ex eb, Ex ec, Ex tb and Ex tc. The motors are made with a highly robust design comprising an enclosure and bearing plates in grey cast iron and a fan cover in steel. The high level of efficiency (class IE3) and easy-maintenance design mean low operating costs for the user. A number of pre-defined industry-specific options are available such as special coatings with category C4 high-level corrosion protection, stainless steel screws and bolts or extended warranty periods which enable these motors to be used in the chemical or oil and gas sectors, with the option to add freely selectable features such as reduced start-up current, motor monitoring, reinforced bearings or tropical climate versions with paint finish versions up to category C5-M for offshore applications. The standardized documentation is flexibly configured to allow adaptation to both simple and highly complex projects.
With its integrated Simotics XP platform for explosion-proof motors, Siemens offers a reliable, simple and rapid solution to the achievement of greater safety. With its technically seamless concept, the motor series covers all kinds of potentially explosive zones. They are available for either mains or converter-fed operation and in various efficiency classes up to IE3 without jumps in shaft height, while ensuring environmentally low-impact operation and a rapid return on investment.
For further information on Simotics XP, please see www.siemens.com/simotics-xp
Find further information about Siemens at the Achema 2018 at www.siemens.com/achema and www.siemens.com/press/achema2018
For this press release
Event: Achema 2018
Press Event
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 377,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Stefan Rauscher
Siemens AG
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (911) 895-7952