Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release12 May 2017Power and GasErlangen
First turbines for expansion of Bolivian power plants start their journey

"With this project we achieve the fastest, most efficient and most cost-effective expansion of the power generating capacities in Bolivia," stated Willi Meixner, CEO of Siemens Power and Gas Division. "The country will save a lot of natural gas by the distinct increase of efficiency of the three power plants. And of course also the environment will benefit. Modern technologies will make a significant contribution to improve access to electricity for the growing population and the developing economy."
Two industrial gas turbines started their journey over the Atlantic Ocean and through the Panama Canal. After landing at the Arica port in Chile, the cargo will be loaded on a truck to travel the remaining 1,800 kilometers to the construction site at Termoeléctrica del Sur on overland route crossing the Andes at a height of 4680 meters. The slightly developed road network, rough terrain and extreme weather conditions are the main challenges for the overland transports. The two gas turbines will be installed to drive the electrical generators and produce steam to drive the steam turbine and thus increasing the efficiency of the power plant to more than 50 percent.
Cristian León, Operations Manager of Ende Andina and Site Manager of the combined cycle expansion project, expressed his satisfaction with the departure of the first turbines: "We are also prepared on site to receive these turbines, since the foundations of both turbines and generators are ready with much time in advance to ensure that on arrival they can be placed on their foundation and that the assembly process can run within the established schedule. Thanks to the civil works activities carried out in our three plants we ensure that the project will not suffer any delays".
Siemens will supply 14 industrial gas turbines, eleven steam turbines and further power plant equipment to expand the Termoeléctrica del Sur, Termoeléctrica de Warnes and Termoeléctrica Entre Rios plants for combined cycle operation. With the expansion projects, Siemens and its Spanish consortium partner TSK are adding more than one gigawatt to the Bolivian power grid. The projects will increase the installed power generating capacity of Bolivia's National Interconnected System by 66 percent, provide a reliable energy supply for the local population and lay the foundation for a possible electricity export.
For further information and material on Siemens energizing Bolivia, please see www.siemens.com/press/energizing-bolivia
For further information on Siemens' Power and Gas Division, please see: www.siemens.com/about/power-gas
For this press release

Infographic: Energizing Bolivia
Infographic: Energizing Bolivia
Update
This press release was updated on 19.05.2017 at 04:00 PM CEST.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Alfons Benzinger
Siemens AG
Freyeslebenstr. 1
91058 Erlangen
Germany
91058 Erlangen
Germany
+49 (9131) 18-7034