Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release03 September 2019Digital IndustriesNuremberg
Digital junction box - increased transparency in monitoring and diagnostics

The seamless connection of the control unit and Siwarex WP weighing electronic enables immediate diagnostics of the load cells. This makes servicing quicker and easier, and minimizes downtimes. In order to prevent inaccurate or incorrect measurements, the weighing modules must operate precisely. An essential requirement for this is complete transparency regarding the status of the devices. Siwarex DB offers the option of connecting the scales with up to four load cells, thus providing the required flexibility in plant planning. A new feature is the single-channel monitoring of each connected load cell. For example, error conditions such as wire break or overload can be detected and removed specifically, making servicing easier. With Siwarex DB, the use of a multimeter is a thing of the past. Siwarex DB can also be used in a wide range of applications in the field of industrial weighing technology, such as level monitoring, silo or container weighing.
By using a Siwarex WP231 as the weighing electronic, direct connection to a Simatic S7 CPU for the Simatic S7-1200 system is supported. For the distributed Simatic ET 200SP system, on the other hand, the use of Siwarex WP321 is recommended. Seamless communication between Siwarex and Simatic reduces effort during commissioning. If, for example, height compensation is required during commissioning, the load of each individual load cell can be viewed immediately using the Siwarex WP weighing electronics.
The Siwarex DB digital junction box can be used to retrofit existing plants with minimal effort. If the similar Siwarex JB solution is already in use, it can be simply replaced with the Siwarex DB (which has the same dimensions) and connected to the existing cables. Another advantage for the user is that there is no change to the normal operating procedures within the Siwarex weighing electronics and Simatic.
For this press release
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI's unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 75,000 employees internationally.
Siemens AG
(Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of power generation and distribution, intelligent infrastructure for buildings and distributed energy systems, and automation and digitalization in the process and manufacturing industries. Through the separately managed company Siemens Mobility, a leading supplier of smart mobility solutions for rail and road transport, Siemens is shaping the world market for passenger and freight services. Due to its majority stakes in the publicly listed companies Siemens Healthineers AG and Siemens Gamesa Renewable Energy, Siemens is also a world-leading supplier of medical technology and digital healthcare services as well as environmentally friendly solutions for onshore and offshore wind power generation. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at
www.siemens.com.
Reference Number: PR201908295339en
Contact
Katharina Zoefeld
Digital Industries
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (172) 5876725