Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release28 February 2017Building TechnologiesZug
Desigo Control Point – building monitoring and operation made easy

Desigo Control Point – building monitoring and operation made easy
Desigo Control Point makes it possible to operate building systems from an easy to use graphical user interface, on any device. It is suitable for everything from room operation and dashboards to the operation and monitoring of the primary system. Depending on the field of application and customer requirements, different technologies can be used to connect them to the disciplines to be controlled. The TCP/IP touch panels are suitable for projects where multiple panels access the same data served by a central web interface, for example in conference rooms or open-plan offices. In contrast, the BACnet/IP touch panels can be deployed standalone in the BACnet network. The BACnet/IP touch panel includes a web interface for remote operation using a standard web browser on third-party devices.
Desigo Control Point also offers tools to visualize, monitor and optimize energy consumption. For example, it is possible to create energy dashboards for managing and analyzing the energy footprint of the monitored systems or to display consumption trends to the public. The most important data is logged continuously, allowing optimization measures to be implemented based on historical data and derived trends. Collected data can also be exported for further analysis.
Other Desigo Control Point features are alarm forwarding via e-mail and SMS, creation of schedules, and simplified reporting. Finally, Desigo Control Point has an integrated graphics editor and an extensive library with templates and symbols. The solution can display 2D and 2D+ symbols and graphics statically or as animations. Desigo Control Point supports tool-free commissioning.
Desigo Control Point is suitable not only for smaller and medium-sized HVAC projects, but also for room automation projects and projects requiring highly customized user interfaces. The new solution will be available in the second half of the year.
For further information on the Building Technologies Division, please see www.siemens.com/buildingtechnologies
For further information on Desigo, please see www.siemens.com/desigo
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.