Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release22 November 2017Digital Factory Nuremberg
All-round IP65-protected Panel and Panel PC for user-friendly operator control and monitoring

The picture shows the Simatic HMI TP1200 Comfort Panel PRO with 12-inch display diagonal.
For powerful, PC-based HMI applications, the technology of the improved E generation of industrial Panel PCs is installed in the Simatic IPC477E PRO Panel PC – with 6th generation Intel Core i processor and modern Celeron and Xeon processors. The new Panel PC has a wide range of interfaces, such as 3x Gigabit Ethernet, 4x USB 3.0 and optional 2x COM to facilitate flexible use. Extension units –mountable components – extend the operation of the all-round IP65-protected PRO devices. The 12 to 22-inch extension units, which consist of standard components such as basic device, extension components, mounting adapters, keyboard tray and an optional keyboard also available in IP65 stainless steel versions, allow tailor-made system solutions. They are characterized by easy mounting and commissioning, as well as user-friendly engineering, and can be easily adapted to meet individual customer requests. A large selection of control elements is also available: from indicator lights, selector and key switches, Emergency OFF mushroom pushbuttons, USB interface and RFID reader, all the way to a stainless-steel keyboard. The control elements are easily and quickly labeled with label holders and inscription plates, or inscription plates and lens assemblies. The extension unit is now also available in a fail-safe Profisafe version, in addition to the conventionally hard-wired and bus-capable Profinet version.
For further information, refer to www.siemens.com/simatic-hmi-pro
Further information about Siemens at the SPS IPC Drives 2017 at www.siemens.com/sps-ipc-drives and www.siemens.com/press/sps2017
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 372,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Gerhard Stauss
Siemens AG
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (911) 895-7945