Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release31 January 2019Siemens Mobility GmbHMunich
56 regional trains for Augsburg rail networks

"We are especially pleased to begin operating our fifth network in Germany – Lot 1 of the Augsburg networks. The state-of-the-art trains being supplied by our partner Siemens Mobility are an important building block for ensuring high-quality operations that will attract additional passengers to rail transport," said Stefan Krispin, CEO of Go-Ahead Verkehrsgesellschaft Deutschland GmbH.
"This is yet another order for our two regional train platforms in our key home market. For the first time, we'll be delivering the trains so both types can be combined in operation. This way, the strengths of both train types can be optimally utilized," said Sabrina Soussan, CEO of Siemens Mobility.
The trains are designated for service on the routes Ulm – Augsburg – Munich, Würzburg – Ansbach – Treuchtlingen – Donauwörth – Augsburg as well as Aalen – Nördlingen – Donauwörth. All of the trains are designed to meet projected increasing traffic demand in the region. In particular, the double-decker trains planned for routes to and from Munich will provide a substantial increase in seating capacity.
The Mireo offers 216 and the Desiro HC 538 seats. To further increase flexibility in meeting passenger demand, up to four three-car Mireos can be combined as a train or a maximum of two Mireos combined with a Desiro HC. If even more capacity is needed, two Desiro HC trainsets can be coupled. A multipurpose area is located at each car doorway; 18 bicycles can be transported in a Mireo and 45 in a Desiro HC. All trains are barrier-free for passengers with limited mobility. The trains also have a lift on board in order to provide wheelchair users easy access at stations with low platforms.
A real-time passenger information system shows arrival and departure times as well as connections at the respective stations. The trains are equipped with high-frequency window glass specially developed by Siemens Mobility to substantially improve mobile reception. In addition, the trains will be prepared for a possible later installation of WLAN technology.
For this press release

@SiemensMobility
Go-Ahead Verkehrsgesellschaft Deutschland GmbH is a subsidiary of the British company Go-Ahead, one of the leading providers of public transport by bus and train. In the UK, Go-Ahead transports about 30 percent of all rail passengers and more than two million passengers per day through various regional bus companies. Sustainability and security are central corporate values that are lived out in everyday work. This is proven by the Carbon Trust Triple Standard for waste recycling, water-saving and climate-friendly commitment. www.go-ahead-bahn.de.
Siemens Mobility is a separately managed company of Siemens AG. As a leader in transport solutions for more than 160 years, Siemens Mobility is constantly innovating its portfolio in its core areas of rolling stock, rail automation and electrification, turnkey systems, intelligent traffic systems as well as related services. With digitalization, Siemens Mobility is enabling mobility operators worldwide to make infrastructure intelligent, increase value sustainably over the entire lifecycle, enhance passenger experience and guarantee availability. In fiscal year 2018, which ended on September 30, 2018, the former Siemens Mobility Division posted revenue of €8.8 billion and had around 28,400 employees worldwide. Further information is available at: www.siemens.com/mobility.