Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Siemens Mobility and ÖBB digitize Austria’s rail network
At a press conference held in Linz today, Siemens Mobility and ÖBB-Infrastruktur AG presented a framework agreement for a long-term cooperation and announced the successful commissioning of a first route section. The agreement regulates the expansion of the ETCS Level 2 system throughout Austria’s high-level rail network, the establishment of so-called ETCS Radio Block Centers or RBCs, which will be redundant, and the maintenance and servicing of these facilities. During the project’s rollout, plans call for installing a total of 21 RBCs by 2038 to provide fail-safe coverage for Austria’s high-level rail network.
“Efficient railway infrastructure is critically important for achieving Austria’s climate goals. To help us handle the expected increase in rail traffic and shift away from roads, we are relying extensively on digital initiatives, and ETCS Level 2 is an enormously important component for railways of the future. The framework agreement signed with Siemens Mobility is based on a Europe-wide tender and we’re looking forward now to working with the best bidder to equip further rail routes with Level 2.”
“We are proud to be working with ÖBB to equip the Austrian rail network with ETCS Level 2, and the commissioning of this route marks an important milestone in ÖBB’s continuing expansion of ETCS coverage. The use of ETCS Radio Block Centers and our innovative software-based DS3 safety platform will significantly increase route capacity and make the Austrian railway system one of the most modern in the world.”
With ETCS Level 2, data is transmitted from the ETCS Radio Block Center to trains via GSM-R train radio. Data balises in the tracks are used to determine a train’s position and relay unalterable route data. The corresponding interlocking transmits track vacancy data and other information to the RBC. The RBC then generates the driving permit and sends it to the train. This continuous bidirectional flow of data considerably increases the line throughput. Driving trains with this “electronic vision” through several track blocks allows shorter headways at maximum speeds.
DS3 stands for “Distributed Smart Safe System” and is the new software platform from Siemens Mobility for safety-relevant logic. The platform is used to migrate existing applications such as ETCS or interlockings to a standard high-performance platform based on COTS, which uses multicore technology and a new communication concept for a fully IP-based system architecture. DS3 will enable ETCS control centers to be further optimized and given greater flexibility.
For this press release
Follow us on Twitter
Siemens Mobility is a separately managed company of Siemens AG. As a leader in intelligent transport solutions for more than 175 years, Siemens Mobility is constantly innovating its portfolio. Its core areas include rolling stock, rail automation and electrification, a comprehensive software portfolio, turnkey systems as well as related services. With digital products and solutions, Siemens Mobility is enabling mobility operators worldwide to make infrastructure intelligent, increase value sustainably over the entire lifecycle, enhance passenger experience and guarantee availability. In fiscal year 2022, which ended on September 30, 2022, Siemens Mobility posted revenue of €9.7 billion and had around 38,200 employees worldwide. Further information is available at: www.siemens.com/mobility.