Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release13 September 2023Digital IndustriesNuremberg
Siemens Xcelerator: New functions for Sinumerik One increase performance and contribute to a more sustainable production
With the new Sinumerik software version V6.22, there are new technology functions for the Sinumerik One that increase transparency in the machine, simplify operation, reduce machine wear, and increase performance.
Sinumerik Ctrl-E in V6.22 with new functions
With the simple and well-established Ctrl-E key combination on the control panel, Sinumerik One enables a quick evaluation of the machine's energy consumption. The function enables visualization of the most important energy consumption factors and simple creation as well as management of machine profiles. New in software version V6.22 is the function for optimized spindle acceleration (Balanced Spindle Acceleration). The spindle acceleration is automatically adjusted so that the programmed spindle speed is only reached when required. This reduces the acceleration current and the thermal losses of the spindle motor, which in turn saves electrical energy during spindle operation. This is particularly beneficial when there are many tool changes. In addition, reducing the spindle acceleration to the necessary minimum also reduces the mechanical load, which increases the service life of the spindle.
Flexible HMI portfolio for multifunctional machine tools
Simple and intuitive operation is the top priority for the Sinumerik One HMI portfolio. With the scalable portfolio of 15 to 24 inch multi-touch panels and the matching machine control panels, the requirements of modern multifunctional machine tools for flexibility and adaptability are met. New to the portfolio are the Sinumerik One Machine Control Panels (MCPs) 1900 plus, 1500 and the matching QWERTY keyboards. Not only in hardware, but also in software, the focus is on flexibility and customization. The Sinumerik Operate Display Manager makes it easy to implement a customizable interface that not only adapts to the various display sizes, but also to the individual needs of the machine operator. The Display Manager allows videos and PDFs, for example, to be displayed clearly in various customizable layouts. To meet the ever-increasing performance requirements of the HMI software, the new IPC generations (Simatic IPC 2x7G and Simatic IPC BX/PX-39A) will be used in the future. The additions to the Sinumerik One HMI portfolio guarantee a consistent and scalable hardware concept.
Perfect compatibility in use and programming
Sinumerik One not only offers numerous advantages over its predecessor Sinumerik 840D sl but is also perfectly compatible in use and programming. This not only eliminates the need for retraining for the operator, but also allows programs and cycles to be reused. This saves costs and facilitates the introduction of the new generation of machines.
Further information regarding Siemens at EMO 2023 are available at
www.siemens.com/press/emo23 und
www.siemens.com/emo
For this press release
Follow us on Social Media
Siemens Digital Industries DI is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions, and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 72,000 employees internationally.
Siemens AG (Berlin and Munich) is a technology company focused on industry, infrastructure, transport, and healthcare. From more resource-efficient factories, resilient supply chains, and smarter buildings and grids, to cleaner and more comfortable transportation as well as advanced healthcare, the company creates technology with purpose adding real value for customers. By combining the real and the digital worlds, Siemens empowers its customers to transform their industries and markets, helping them to transform the everyday for billions of people. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a globally leading medical technology provider shaping the future of healthcare. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the transmission and generation of electrical power.
In fiscal 2022, which ended on September 30, 2022, the Siemens Group generated revenue of €72.0 billion and net income of €4.4 billion. As of September 30, 2022, the company employed around 311,000 people worldwide. Further information is available on the Internet at www.siemens.com.
In fiscal 2022, which ended on September 30, 2022, the Siemens Group generated revenue of €72.0 billion and net income of €4.4 billion. As of September 30, 2022, the company employed around 311,000 people worldwide. Further information is available on the Internet at www.siemens.com.